Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZUBoard Using the Zuboard syzygy ports
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 363 subscribers
  • Views 934 views
  • Users 0 members are here
Related

Using the Zuboard syzygy ports

loukilitarik2020
loukilitarik2020 over 1 year ago

Hi,

I'm trying to use a few PMODs sensors with the Zuboard, any recommendations on how to achieve that. I already bought the SZG-PMOD4 (Opal Kelly) but it didnt work for me.

Thanks

Tarik

  • Sign in to reply
  • Cancel
  • iksevas
    0 iksevas over 1 year ago

    You will need to use the HSIO standard or TXR2 with PMOD voltage of 1.8V because of ZUBoard HP bank signal levels.

    The Syzygy PMOD board is looking for VIO of 3.3V which ZUboard will not provide. So either you have no voltage provided to PMOD connector if add-on card is blocking that voltage or you have 1.2V/1.8V from  ZUBoard which may not power your PMOD which requires 3.3V.

    A properly designed add-on board would require level translation to support  all of the voltages.

    You may be better off using MikroE Click to PMOD but this is IO limited so you won’t get as many PMODs..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • loukilitarik2020
    0 loukilitarik2020 over 1 year ago in reply to iksevas

    i think you are correct, it is a voltage level problem. are you aware of any expansion board with a voltage level translation for these Syzygy ports 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • iksevas
    0 iksevas over 1 year ago in reply to loukilitarik2020

    Unfortunately I do not.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • loukilitarik2020
    0 loukilitarik2020 over 1 year ago

    Anyone here can help provide a simple schematic example to expose the syzgy pins as a 3.3v level ios. Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dyessgg
    0 dyessgg over 1 year ago in reply to loukilitarik2020

    Digilent has voltage level shifters for the PMOD side.  You might look into those to see if that can be used.  I find it odd that someone would put out a SZG to PMOD adapter and not include DC-DC converters for the supply voltage and level shifters for the signal lines.