Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZUBoard ZUBoard PYNQ with eMMC and SSD - an easier way?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 363 subscribers
  • Views 757 views
  • Users 0 members are here
  • ssd
  • ZU Board 1CG
  • emmc
  • pynq
  • kernel
  • m.2
  • ZUBoard
  • boot
  • zub1cg
  • zu1cgboard
Related

ZUBoard PYNQ with eMMC and SSD - an easier way?

tjaekel
tjaekel over 1 year ago

I was thinking...:
is there an easier way to add and enable eMMC (and even SSD/M.2 module) for ZUBoard running PYNQ?

Potentially, there is!

Tests done:

If I image SD card with PYNQ image, boot it, afterwards I copy/overwrite the BOOT.bin and image.ub with the one from a PetaLinux image
(used to demonstrate that eMMC and SSD/M.2 works):
- oh, yes, I see eMMC and even nvme device
- I can mount and use: all looks fine

BUT:
the FPGA Manager is not enabled!
So, even PYNQ seems to boot fine - just: it cannot load any overlay.bit file!
Obvious: the FPGA Manager is not enabled, not added in the (BSP and) PetaLinux kernel.

So, what about to build a new PetaLinux kernel for the ZUBoard (only the kernel, not all, not the entire PYNQ image)?

I assume,

  • if you use a newer BSP, e.g. "zub1cg_sbc_base_2022_2.bsp", not the original one used in ZUBoard PYNQ build as "zuboard_1cg.bsp"
  • you build just the PetaLinux kernel and u-boot
  • but before the build: you configure the PetaLinux project to enable/add the FPGA Manager (petalinux-config)

maybe, it is enough to exchange the kernel (image.ub, and UBOOT.BIN) so that:

  • a PYNQ SD Card (with patched BOOT.BIN and image.ub) boots fine
  • sees also if eMMC module is connected
  • sees also if SSD/M.2 module is connected instead (and you can mount SSD/M.2 as a drive in system)
  • and you can also load dynamically custom overlay.bit files

So, I think:

supporting eMMC or SSD/M.2 is just an issue with the PetaLinux kernel (image.ub) itself:
changing the kernel with one supporting both (optional) devices, but having also FPGA Manager enabled in it...
should do the job.

Just: build a PetaLinux image based on a newer BSP repository, change the files on the PYNQ image (e.g. after system has booted,
to overwrite the BOOT.BIN and esp. image.ub)... and it should be done.

I am testing this approach right...

Please:
can anybody generate a PetaLinux kernel (image.ub) which would support eMMC and SSD/M.2?
It should be OK to image SD card with original PYNQ image but after it has booted - to overwrite (patch) these files,
so that is sees both devices and still works to load custom overlay.bit files in Python.
It should not be big deal.

  • Sign in to reply
  • Cancel
Parents
  • tjaekel
    0 tjaekel over 1 year ago

    It is not yet working:
    I get build errors...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • tjaekel
    0 tjaekel over 1 year ago

    It is not yet working:
    I get build errors...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • tjaekel
    0 tjaekel over 1 year ago in reply to tjaekel

    But, for now, at least to get eMMC working:

     ZUBoard PYNQ - patch for eMMC support 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tjaekel
    0 tjaekel over 1 year ago in reply to tjaekel

    please see here:

    community.element14.com/.../zuboard-with-ssd-m-2-and-pynq---works

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer