Azure Sphere Starter Kit
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Azure Sphere Starter Kit
  • More
  • Cancel
Azure Sphere Starter Kit
Forum Rude awakening
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Azure Sphere Starter Kit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 56 subscribers
  • Views 2785 views
  • Users 0 members are here
  • azure sphere
Related

Rude awakening

rsc
rsc over 7 years ago

I received this today:

image

So now I have to choose to continue this project and pay Microsoft, or quit and work on something else.

Here's my "Free Trial" cost analysis:

image

So....if I choose to continue to work on this project for another month, it will cost me approx $150 without changing any features.

I'm not sure its worth the price just to enter a contest.

Scott

  • Sign in to reply
  • Cancel

Top Replies

  • kmikemoo
    kmikemoo over 7 years ago +4
    I have received something similar. Let me lead with "Go slow. It doesn't have to cost you anything." When I signed up for my "free" account, I used my hotmail.com account - because it's a Microsoft account…
  • shabaz
    shabaz over 7 years ago in reply to colporteur +4
    Hi Sean, All the cloud providers have billing that sometimes takes a while to get the head around, not because they're intentionally trying to get the casual user testing their system to pay huge fees…
  • rsc
    rsc over 7 years ago in reply to javagoza +3
    If you want to save data and plot the data a "Time Series Insights environment" attached to your IoT Hub is $150 /month using default options. If you click on pay-as-you-go, you get different pricing.…
Parents
  • ducktail
    ducktail over 7 years ago

    My credit card was charged when I registered, according to Microsoft it would be reverse at the end of the month. Will monitor that to ensure the reversal is done.

     

    After playing with the board I realized that the  free subscription will be used up really fast  if we are not careful. If this were to go into production you will have a few hundreds or worst  a few thousands of these boards deployed as one of my customer pointed out.

     

    So my testing would Really determine whether it's feasible to go with this board or some other SBC/microcontroller that doesn't use Microsoft Products( restricted for now).  And implement some other security like WoTT.

     

    Just my personal observations  after testing..........

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 7 years ago in reply to ducktail

    Your observations provide insight into an incremental costs that would come into play post development for a production solution. The total cost of ownership (TCO) for such a solution would need to include the data overhead costs.

     

    Is the Azure solution restricted to just the MS portal or does the technology permit other opportunities? I ask because I don't have any insight. I elected to not participate in the offering. In the end Canada was not supported in the trial.

     

    I make it a point to closely examine TCO for a solution I have found sometimes the sticker price for implementation is attractive but the ongoing costs can be crippling. Especially when the pricing is per unit deployment.

     

    I recall implementing a vendor solution that included 25K licenses. No one asked about the costs posts 25K. After being in production for two years the initial license block was consumed and the size of addition license blocks was smaller with the costs incrementally higher. What could you do when you are locked into the solution!

     

    Something designers should be aware of. IoT solutions for ten development units verses 10K production units can exhaust a budget real fast.

     

    Sean

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • colporteur
    colporteur over 7 years ago in reply to ducktail

    Your observations provide insight into an incremental costs that would come into play post development for a production solution. The total cost of ownership (TCO) for such a solution would need to include the data overhead costs.

     

    Is the Azure solution restricted to just the MS portal or does the technology permit other opportunities? I ask because I don't have any insight. I elected to not participate in the offering. In the end Canada was not supported in the trial.

     

    I make it a point to closely examine TCO for a solution I have found sometimes the sticker price for implementation is attractive but the ongoing costs can be crippling. Especially when the pricing is per unit deployment.

     

    I recall implementing a vendor solution that included 25K licenses. No one asked about the costs posts 25K. After being in production for two years the initial license block was consumed and the size of addition license blocks was smaller with the costs incrementally higher. What could you do when you are locked into the solution!

     

    Something designers should be aware of. IoT solutions for ten development units verses 10K production units can exhaust a budget real fast.

     

    Sean

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Children
  • shabaz
    shabaz over 7 years ago in reply to colporteur

    Hi Sean,

     

    All the cloud providers have billing that sometimes takes a while to get the head around, not because they're intentionally trying to get the casual user testing their system to pay huge fees, but just simply because the casual user is using the exact same system as the people building large services.

     

    They don't mostly mind the casual user with their few hundred requests a month, because they want them to build up to hundreds of thousands of requests a month. My monthly AWS bill is tiny, I only use it to test a few features from time to time.

     

    Once with AWS as an individual I had a huge bill ($200 for a month), but it was my fault - I was using IaaS (i.e. dedicating resources for myself), and I powered up a massive machine, and forgot to turn it off : ( In that respect, the IoT solutions from Amazon, Microsoft etc can be cheaper for the causal experimenter or design engineer, since it is PaaS which is not dedicating (much) computing resources until they are needed. Taken to the extreme, there's the possibility of consuming zero computing power until customers come along, using so-called FaaS (function-as-a-service). With that, provided you're not using other billable things to design the solution (e.g. large databases) then there is zero cost (or near-zero, since it depends on how the service provider wants to handle it) and you only incur cost that grows as usage of the service grows. AWS offer that, Azure will have a similar thing.

     

    Using typical third party software IP in code can (sometimes) initially cost heaps more than an IoT solution from the SPs, depending on how specialist or desirable it is. They like older licensing schemes, e.g. a block of licenses, so there is a larger up-front cost.

     

    The IoT solutions are more granular, at least the ones I've encountered, to encourage developers to test them out with zero or near-zero cost, and then ramp up.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 7 years ago in reply to shabaz

    I have limited experience developing systems outside a closed environment. Closed in the sense the systems were within a network the company owned and managed. As an ISP provider the network was large and 100K of devices. Not big to US standards but large in Canada.

     

    In the true sense of IoT, the client (i.e. IoT device) could be in any network. Finding an IoT data collector that has a reach into the expanse of any everywhere network would be daunting. I can only imagine the claims of vendors to garner business. Proving the claims would be a task.

     

    Providers of the service and costing models piques my interest. I have to confess, I can have an interest knowing the details but am relieved I won't be part of a team trying to deliver.

     

    Sean