Azure Sphere Starter Kit
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Azure Sphere Starter Kit
  • More
  • Cancel
Azure Sphere Starter Kit
Forum Pluton
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Azure Sphere Starter Kit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 52 subscribers
  • Views 1677 views
  • Users 0 members are here
Related

Pluton

wizio
wizio over 7 years ago

what is it used for

 

PLUTON_GET_SECURITY_STATE
PLUTON_GENERATE_CLIENT_AUTH_KEY
PLUTON_COMMIT_CLIENT_AUTH_KEY
PLUTON_GET_TENANT_PUBLIC_KEY
PLUTON_PROCESS_ATTESTATION
PLUTON_SIGN_WITH_TENANT_ATTESTATION_KEY
PLUTON_SET_POSTCODE
PLUTON_GET_BOOT_MODE_FLAGS
PLUTON_IS_CAPABILITY_ENABLED
PLUTON_GET_ENABLED_CAPABILITIES
PLUTON_SET_MANUFACTURING_STATE
PLUTON_GET_MANUFACTURING_STATE




SECURITY_MONITOR_WRITE_LOG
SECURITY_MONITOR_GET_LOG_DATA
SECURITY_MONITOR_SMAPI_COMMAND (API)
SECURITY_MONITOR_DERIVE_KEY
SECURITY_MONITOR_GET_PERIPHERAL_COUNT
SECURITY_MONITOR_LIST_PERIPHERALS
SECURITY_MONITOR_LIST_PERIPHERALS_V1
SECURITY_MONITOR_ENABLE_PERIPHERAL_DRIVER
SECURITY_MONITOR_IO_CORE_CONTROL
SECURITY_MONITOR_RECORD_TELEMETRY_EVENT_DATA
SECURITY_MONITOR_GET_TELEMETRY
SECURITY_MONITOR_RESET_RETAIN_TELEMETRY




SECURITY_MONITOR_API_GET_VERSION 
SECURITY_MONITOR_API_PING 
SECURITY_MONITOR_API_QUERY_FLASH 
SECURITY_MONITOR_API_ERASE_FLASH 
SECURITY_MONITOR_API_WRITE_FLASH 
SECURITY_MONITOR_API_VERIFY_IMAGE_BY_FLASH_ADDRESS_CMD 
SECURITY_MONITOR_API_RESET_CMD 
SECURITY_MONITOR_API_WRITE_LOG 
SECURITY_MONITOR_API_GET_LOG_DATA_SIZE 
SECURITY_MONITOR_API_GET_LOG_DATA 
SECURITY_MONITOR_API_DERIVE_KEY_CMD 
SECURITY_MONITOR_API_GET_PERIPHERAL_COUNT 
SECURITY_MONITOR_API_LIST_PERIPHERALS 
SECURITY_MONITOR_API_GET_WIFI_FIRMWARE_LOCATION 
SECURITY_MONITOR_API_GET_APPLICATION_IMAGE_COUNT 
SECURITY_MONITOR_API_LIST_ALL_APPLICATION_IMAGES 
SECURITY_MONITOR_API_SHOULD_IMAGE_BE_UPDATED 
SECURITY_MONITOR_API_INVALIDATE_IMAGE 
SECURITY_MONITOR_API_OPEN_IMAGE_FOR_STAGING 
SECURITY_MONITOR_API_WRITE_BLOCK_TO_STAGE_IMAGE 
SECURITY_MONITOR_API_COMMIT_IMAGE_STAGING 
SECURITY_MONITOR_API_ABORT_IMAGE_STAGING 
SECURITY_MONITOR_API_INSTALL_STAGED_IMAGES 
SECURITY_MONITOR_API_GET_COMPONENT_COUNT 
SECURITY_MONITOR_API_GET_COMPONENT_SUMMARY 
SECURITY_MONITOR_API_GET_COMPONENT_IMAGES 
SECURITY_MONITOR_API_STAGE_COMPONENT_MANIFESTS 
SECURITY_MONITOR_API_COUNT_OF_MISSING_IMAGES_TO_DOWNLOAD 
SECURITY_MONITOR_API_GET_MISSING_IMAGES_TO_DOWNLOAD 
SECURITY_MONITOR_API_SET_PERIPHERAL_MAPPING 
SECURITY_MONITOR_API_SET_PIN_MAPPING 
SECURITY_MONITOR_API_GET_ABI_TYPE_COUNT 
SECURITY_MONITOR_API_GET_ABI_VERSIONS 
SECURITY_MONITOR_API_SET_RTC_CURRENT_TIME 
SECURITY_MONITOR_API_SET_RTC_ALARM 
SECURITY_MONITOR_API_GET_UPDATE_CERT_STORE_IMAGE_INFO 
SECURITY_MONITOR_API_STAGE_BASE_MANIFESTS 
SECURITY_MONITOR_API_COUNT_OF_MISSING_BASE_IMAGES_TO_DOWNLOAD 
SECURITY_MONITOR_API_GET_MISSING_BASE_IMAGES_TO_DOWNLOAD 
SECURITY_MONITOR_API_IO_CORE_CONTROL 
SECURITY_MONITOR_API_GET_ROLLBACK_INFO 
SECURITY_MONITOR_API_RECORD_TELEMETRY_EVENT_DATA 
SECURITY_MONITOR_API_GET_TELEMETRY_DATA 
SECURITY_MONITOR_API_RESET_TELEMETRY 
SECURITY_MONITOR_API_RETAIN_TELEMETRY

  • Sign in to reply
  • Cancel

Top Replies

  • wizio
    wizio over 7 years ago in reply to clem57 +1
    oo I have questions - What is Telemetry and why is protected from pluton
  • bwilless
    bwilless over 7 years ago in reply to wizio +1
    When an Azure Sphere MCU is produced at the silicon factory, a private/public key pair is generated in the silicon. The private key is stored in the silicon is only accessible to the Pluton security sub…
  • wizio
    wizio over 7 years ago in reply to bwilless +1
    You're wrong and here Manufacturing_GetDeviceId () libapplibs.so (full version) return attestation_public_key[] - TESTED
Parents
  • wizio
    wizio over 7 years ago

    Example - Get Device ID

    There is hidden function  int Manufacturing_GetDeviceId(char * hex_buffer, int size = 129) libapplibs.so

     

    Reversed Function is:

     

    struct azure_sphere_get_security_state_result

     

    {

      uint32_t state;                     // Security state of device (0x04000000)

      uint8_t general_public_key[64];     // ECC General public key

      uint8_t attestation_public_key[64]; // Attestation public key (is used as DeviceID)

    };


    int get_security_state(struct azure_sphere_get_security_state_result *p)

    {

      if (NULL == p)

        return -1;

      struct azure_sphere_get_security_state_result d;

      int fd = open("/dev/pluton", 0x80000);

      if (fd < 0)

        return -1;

      int err = ioctl(fd, 0xC0847001, &d);

      if (0 == err)

        memcpy(p, &d, sizeof(d));

      else

        memset(p, 0, sizeof(d));

    #if 0

      char *c = (char *)&d;

      printf("[security_state] ");

      for (int i = 0; i < sizeof(d); i++)

        printf("%02X", (int)c[i]);

      printf("\n");

    #endif

      close(fd);

      return err;

    }

     

    so ... Manufacturing_GetDeviceId() return attestation_public_key[64]

    ioctl( 0xC0847001 ) is

    #define PLUTON_GET_SECURITY_STATE _IOWR('p', 0x01, struct azure_sphere_get_security_state_result)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bwilless
    bwilless over 7 years ago in reply to wizio

    When an Azure Sphere MCU is produced at the silicon factory, a private/public key pair is generated in the silicon.  The private key is stored in the silicon is only accessible to the Pluton security sub system.  The public key, is sent to the Azure Sphere Security Service (AS3) so that each device can send encrypted data to  AS3 and since AS3 has the public key, it can decrypt data and also encrypt data to the device.

     

    The public key IS the Azure Sphere Device ID.  

     

    Brian

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • wizio
    wizio over 7 years ago in reply to bwilless

    You're wrong and here

    Manufacturing_GetDeviceId() libapplibs.so (full version)

    return attestation_public_key[] - TESTED

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • bwilless
    bwilless over 7 years ago in reply to wizio

    Looks like you're digging deep!  Thanks for the information.

     

    Brian

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • bwilless
    bwilless over 7 years ago in reply to wizio

    Looks like you're digging deep!  Thanks for the information.

     

    Brian

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • wizio
    wizio over 7 years ago in reply to bwilless

    you are welcome

    just want to check Microsoft security.... nothing else