Azure Sphere Starter Kit
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Azure Sphere Starter Kit
  • More
  • Cancel
Azure Sphere Starter Kit
Forum Is it possible to communicate with PC over USB?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Azure Sphere Starter Kit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 53 subscribers
  • Views 1071 views
  • Users 0 members are here
Related

Is it possible to communicate with PC over USB?

Fred27
Fred27 over 7 years ago

I notice that three USB serial ports appear when the Avnet Azure Sphere Starter Kit is connected to a PC, and I can see these are the listed as the service, recovery and debug ports. It sounds like none of these can be used for user communication, but thought I'd check. I'd rather not add a separate USB to serial if I didn't need one.

  • Sign in to reply
  • Cancel

Top Replies

  • danzima
    danzima over 7 years ago +1
    peterfenn bwilless Hi folks, any insight on the above?
  • Fred27
    Fred27 over 7 years ago in reply to Jan Cumps +1
    I know I can do it with s USB to serial, I was just wondering if it's possible using the built-in one.
Parents
  • Jan Cumps
    Jan Cumps over 7 years ago

    ISU0 should be configurable as a UART and acessible via Click Module 1 and 2.
    You'd need a serial 3V3 to USB converter (a LaunchPad or 3V3 Arduino can do that)

     

     

    image

     

    edit: thre's an example program: https://github.com/Azure/azure-sphere-samples/tree/master/Samples/UART/UART_HighLevelApp

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Fred27
    Fred27 over 7 years ago in reply to Jan Cumps

    I know I can do it with s USB to serial, I was just wondering if it's possible using the built-in one.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 7 years ago in reply to Fred27

    Without a special USB cable no. The PC has USB host interfaces which only talk to USB devices. The USB host interface controls all communications protocols between the host and

    devices. There is no protocol for USB host devices to talk to each other. If you had a USB cable with two device type interfaces connected to each other so they could pass bytes to

    each other and each device interface connected to the host interfaces of the PCs you want to connect together along with the right software then they could talk to each other. I believe

    such cables and software does exist.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • gdstew
    gdstew over 7 years ago in reply to Fred27

    Without a special USB cable no. The PC has USB host interfaces which only talk to USB devices. The USB host interface controls all communications protocols between the host and

    devices. There is no protocol for USB host devices to talk to each other. If you had a USB cable with two device type interfaces connected to each other so they could pass bytes to

    each other and each device interface connected to the host interfaces of the PCs you want to connect together along with the right software then they could talk to each other. I believe

    such cables and software does exist.