Azure Sphere Starter Kit
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Azure Sphere Starter Kit
  • More
  • Cancel
Azure Sphere Starter Kit
Forum Can I use SCP to move a file into Azure Sphere?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Azure Sphere Starter Kit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 15 replies
  • Answers 6 answers
  • Subscribers 53 subscribers
  • Views 2482 views
  • Users 0 members are here
  • azure sphere
Related

Can I use SCP to move a file into Azure Sphere?

clem57
clem57 over 7 years ago

I am wishing to move a configuration file for Azure Sphere. Naturally SCP over SSH would work nicely. Can anyone direct me to a solution? I will have to modify the file sometimes depending on the layout of the equipment in use.

 

Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • bwilless
    bwilless over 7 years ago +3 suggested
    There are a few ways to move configuration data to a Sphere device . . . If you only need to operate on one or two devices you could use a Direct Method call to send down a JSON object with your configuration…
  • wizio
    wizio over 7 years ago in reply to bwilless +3
    4. simple curl download
  • wizio
    wizio over 7 years ago in reply to clem57 +2 suggested
    File System is real but is controled ( firewall ) from Pluton subsytem ... I dont know ( for now ) how to write file ... Pluton is as "dongle" ... hardware "sudo" There is MutableStorage for user ( not…
Parents
  • bwilless
    0 bwilless over 7 years ago

    There are a few ways to move configuration data to a Sphere device . . .

     

    1. If you only need to operate on one or two devices you could use a Direct Method call to send down a JSON object with your configuration:
      1. https://www.element14.com/community/external-link.jspa?url=http%3A%2F%2Favnet.me%2Fazure_sphere_direct_method_blog
    2. If you want to send a file to be included with your application build, you can package the file up into the image_package file.  This Microsoft example (https://github.com/Azure/azure-sphere-samples/tree/master/Samples/ExternalMcuUpdate ) shows how to send a binary file to a Sphere device.  Note that the sample uses the binary file to update a connected MCU, but you can take the file and pull your configuration data.
    3. You could also use device twins to send configuration data to your device.  The OOB examples #2 and #3, use device twins to do things like change the LEDs.

     

    If you only need to operate on a single device, option #3 is simplest.  While option #1 should be easy and give you more flexibility in the structure of your data.

     

    Brian

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • bwilless
    0 bwilless over 7 years ago

    There are a few ways to move configuration data to a Sphere device . . .

     

    1. If you only need to operate on one or two devices you could use a Direct Method call to send down a JSON object with your configuration:
      1. https://www.element14.com/community/external-link.jspa?url=http%3A%2F%2Favnet.me%2Fazure_sphere_direct_method_blog
    2. If you want to send a file to be included with your application build, you can package the file up into the image_package file.  This Microsoft example (https://github.com/Azure/azure-sphere-samples/tree/master/Samples/ExternalMcuUpdate ) shows how to send a binary file to a Sphere device.  Note that the sample uses the binary file to update a connected MCU, but you can take the file and pull your configuration data.
    3. You could also use device twins to send configuration data to your device.  The OOB examples #2 and #3, use device twins to do things like change the LEDs.

     

    If you only need to operate on a single device, option #3 is simplest.  While option #1 should be easy and give you more flexibility in the structure of your data.

     

    Brian

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • wizio
    0 wizio over 7 years ago in reply to bwilless

    4. simple curl download image

    • Cancel
    • Vote Up +3 Vote Down