Azure Sphere Starter Kit
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Azure Sphere Starter Kit
  • More
  • Cancel
Azure Sphere Starter Kit
Forum I2C read bug
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Azure Sphere Starter Kit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 4 answers
  • Subscribers 54 subscribers
  • Views 1761 views
  • Users 0 members are here
Related

I2C read bug

tekmeister
tekmeister over 7 years ago

I'm trying to interface to an I2C device and have uncovered what I think is a major bug in the Azure Sphere I2C libraries.

 

I have opened the I2CMaster, set the speed and try to read from the device:

const uint8_t readLength = 8;
const uint8_t address = 0xD0;
uint8_t b1[20];
uint8_t b2[20];
uint8_t b3[20];
uint8_t b4[20];
uint8_t b5[20];
uint8_t b6[20];


I2CMaster_WriteThenRead(i2cFd, i2cAddress, &address, 1, b1, readLength);
I2CMaster_WriteThenRead(i2cFd, i2cAddress, &address, 1, b2, readLength);
I2CMaster_WriteThenRead(i2cFd, i2cAddress, &address, 1, b3, readLength);
I2CMaster_WriteThenRead(i2cFd, i2cAddress, &address, 1, b4, readLength);
I2CMaster_WriteThenRead(i2cFd, i2cAddress, &address, 1, b5, readLength);
I2CMaster_WriteThenRead(i2cFd, i2cAddress, &address, 1, b6, readLength);

Log_Debug("\nb1[0] = %x, b2[0] = %x, b3[0] = %x, b4[0] = %x, b5[0] = %x, b6[0] = %x\n", b1[0], b2[0], b3[0], b4[0], b5[0], b6[0]);

 

With a readLength of 8 or less, then the content of the output buffers is as expected, and the following is printed to the console:

 

b1[0] = 61, b2[0] = 61, b3[0] = 61, b4[0] = 61, b5[0] = 61, b6[0] = 61

 

However if I make my readLength greater than 8, I get the following console output:

 

b1[0] = 80, b2[0] = 0, b3[0] = 0, b4[0] = 0, b5[0] = 0, b6[0] = 0

 

and my output buffers contain an extra byte before the expected data.

In other words, buffer[0] is rubbish, and my read data is from buffer[1] onwards.

 

If I mix up the readLengths with a combination of values <=8 and > 8, then I discover that the first read of 9 or more bytes is good but subsequent reads of 9 or more bytes are bad with the additional byte at the start, until the next read of 8 or less bytes which is good.

 

Can anyone else reproduce this? I'm using an external I2C device with address 0x77 on the click socket #2.

  • Sign in to reply
  • Cancel

Top Replies

  • tekmeister
    tekmeister over 7 years ago in reply to Fred27 +5 suggested
    Hi David, I did see your issue, but I wasn't sure if it was the same root cause or not. If it is the same problem, then I think I have identified more about the nature of when it happens. My workaround…
  • Fred27
    Fred27 over 7 years ago +3 suggested
    I experienced exactly the same problem. No resolution yet that I know of. Repeated first byte on I2C read with Azure Sphere
  • clem57
    clem57 over 7 years ago +2 suggested
    Start and Stop Condition Each I2C command initiated by master device starts with a START condition and ends with a STOP condition . For both conditions SCL has to be high. A high to low transition of SDA…
Parents
  • jgroman
    0 jgroman over 7 years ago

    I experienced the same problem when trying to port some Arduino drivers. Took me very long time spent debugging and then I blamed it on sensor in question. Reading in smaller chunks works fine.
    Seems that sensor was innocent then.





    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jgroman
    0 jgroman over 7 years ago

    I experienced the same problem when trying to port some Arduino drivers. Took me very long time spent debugging and then I blamed it on sensor in question. Reading in smaller chunks works fine.
    Seems that sensor was innocent then.