Azure Sphere Starter Kit
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Azure Sphere Starter Kit
  • More
  • Cancel
Azure Sphere Starter Kit
Forum I2C read bug
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Azure Sphere Starter Kit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 4 answers
  • Subscribers 54 subscribers
  • Views 1761 views
  • Users 0 members are here
Related

I2C read bug

tekmeister
tekmeister over 7 years ago

I'm trying to interface to an I2C device and have uncovered what I think is a major bug in the Azure Sphere I2C libraries.

 

I have opened the I2CMaster, set the speed and try to read from the device:

const uint8_t readLength = 8;
const uint8_t address = 0xD0;
uint8_t b1[20];
uint8_t b2[20];
uint8_t b3[20];
uint8_t b4[20];
uint8_t b5[20];
uint8_t b6[20];


I2CMaster_WriteThenRead(i2cFd, i2cAddress, &address, 1, b1, readLength);
I2CMaster_WriteThenRead(i2cFd, i2cAddress, &address, 1, b2, readLength);
I2CMaster_WriteThenRead(i2cFd, i2cAddress, &address, 1, b3, readLength);
I2CMaster_WriteThenRead(i2cFd, i2cAddress, &address, 1, b4, readLength);
I2CMaster_WriteThenRead(i2cFd, i2cAddress, &address, 1, b5, readLength);
I2CMaster_WriteThenRead(i2cFd, i2cAddress, &address, 1, b6, readLength);

Log_Debug("\nb1[0] = %x, b2[0] = %x, b3[0] = %x, b4[0] = %x, b5[0] = %x, b6[0] = %x\n", b1[0], b2[0], b3[0], b4[0], b5[0], b6[0]);

 

With a readLength of 8 or less, then the content of the output buffers is as expected, and the following is printed to the console:

 

b1[0] = 61, b2[0] = 61, b3[0] = 61, b4[0] = 61, b5[0] = 61, b6[0] = 61

 

However if I make my readLength greater than 8, I get the following console output:

 

b1[0] = 80, b2[0] = 0, b3[0] = 0, b4[0] = 0, b5[0] = 0, b6[0] = 0

 

and my output buffers contain an extra byte before the expected data.

In other words, buffer[0] is rubbish, and my read data is from buffer[1] onwards.

 

If I mix up the readLengths with a combination of values <=8 and > 8, then I discover that the first read of 9 or more bytes is good but subsequent reads of 9 or more bytes are bad with the additional byte at the start, until the next read of 8 or less bytes which is good.

 

Can anyone else reproduce this? I'm using an external I2C device with address 0x77 on the click socket #2.

  • Sign in to reply
  • Cancel

Top Replies

  • tekmeister
    tekmeister over 7 years ago in reply to Fred27 +5 suggested
    Hi David, I did see your issue, but I wasn't sure if it was the same root cause or not. If it is the same problem, then I think I have identified more about the nature of when it happens. My workaround…
  • Fred27
    Fred27 over 7 years ago +3 suggested
    I experienced exactly the same problem. No resolution yet that I know of. Repeated first byte on I2C read with Azure Sphere
  • clem57
    clem57 over 7 years ago +2 suggested
    Start and Stop Condition Each I2C command initiated by master device starts with a START condition and ends with a STOP condition . For both conditions SCL has to be high. A high to low transition of SDA…
Parents
  • javagoza
    0 javagoza over 7 years ago

    I think you should to check the returned value by the function I2CMaster_WriteThenRead

     

    "Returns: The combined number of bytes successfully written and read, or -1 for failure, in which case errno is set to the error value. A partial result, including a transfer of 0 bytes, is considered a success."

     

    https://docs.microsoft.com/en-us/azure-sphere/reference/applibs-reference/applibs-i2c/function-i2cmaster-writethenread#r…

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • javagoza
    0 javagoza over 7 years ago

    I think you should to check the returned value by the function I2CMaster_WriteThenRead

     

    "Returns: The combined number of bytes successfully written and read, or -1 for failure, in which case errno is set to the error value. A partial result, including a transfer of 0 bytes, is considered a success."

     

    https://docs.microsoft.com/en-us/azure-sphere/reference/applibs-reference/applibs-i2c/function-i2cmaster-writethenread#r…

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • Fred27
    0 Fred27 over 7 years ago in reply to javagoza

    javagoza It's not that the count of the bytes is incorrect, it's the fact that the first byte is repeated. The data is wrong.

     

    The problem seems to occur in both I2CMaster_Read and I2CMaster_WriteThenRead. In my case using a PN7120 NFC reader I have to wait for an IRQ signal between writing and reading so can't use I2CMaster_WriteThenRead anyway.