Monarch Go
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Monarch Go
  • More
  • Cancel
Monarch Go
Forum is there a cmd interface directly to the Monarch?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Monarch Go to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 9 subscribers
  • Views 1472 views
  • Users 0 members are here
  • jafoste4
Related

is there a cmd interface directly to the Monarch?

skruglewicz
skruglewicz over 5 years ago

Hi Everyone and jafoste4 jafoste4

 

I'm reviewing the "AVNET Monarch LTE-M Development Kit" and was wondering if anyone can point me in the right direction to send a command to test if the Modem is connected?

I see that there is AT command interface to for the PI starter kit.

"Launch serial terminal configured with 115200 baud rate, 8 data bit, hardware flow control, no parity, 1 stop bit.

Type ATI1 to get software version and AT+PING=”www.sequans.com” to check connectivity"

 

Can the Monarch Go Arduino Shield work this way? I guess I could try it?

 

Thanks in advance

  • Sign in to reply
  • Cancel

Top Replies

  • jafoste4
    jafoste4 over 5 years ago +1
    Hi Stephen, No there isn't a direct connection to the CMD interface of the Monarch Go in which you can do direct AT commands (not like the Pi Hat). This can be accomplished though by doing a pass through…
Parents
  • jafoste4
    0 jafoste4 over 5 years ago

    Hi Stephen,

     

    No there isn't a direct connection to the CMD interface of the Monarch Go in which you can do direct AT commands (not like the Pi Hat). This can be accomplished though by doing a pass through application in which you send your commands directly through the terminal instance connected to your LPC55S69-EVK passing it to the Monarch Go UART and reading the response.

     

    Unforutnatly I don't have an example code here for you to start with.

     

    -Josh

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 5 years ago

    Hi Stephen,

     

    No there isn't a direct connection to the CMD interface of the Monarch Go in which you can do direct AT commands (not like the Pi Hat). This can be accomplished though by doing a pass through application in which you send your commands directly through the terminal instance connected to your LPC55S69-EVK passing it to the Monarch Go UART and reading the response.

     

    Unforutnatly I don't have an example code here for you to start with.

     

    -Josh

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • skruglewicz
    0 skruglewicz over 5 years ago in reply to jafoste4

    I'll have to ponder this one.

    Pass thru app?

    would I be using stdin? like your using the printf()? which is std out