Monarch Go
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Monarch Go
  • More
  • Cancel
Monarch Go
Forum Monarch Go Documentation
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Monarch Go to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 7 subscribers
  • Views 3790 views
  • Users 0 members are here
  • monarch go
  • monarchgo
Related

Monarch Go Documentation

TMS_Matt
TMS_Matt over 3 years ago

Where can I find the documentation for the Monarch Go module?

I am looking for details specific to the module itself:

  • AT commands reference. I assume most generic AT commands will work, but is there a list of chip specific ones?
  • Mating connector part number and pinout. Mechanical drawings for the module footprint would be helpful too.
  • Electrical specifications. I recall seeing that the UART interface is 1.8v, can anyone confirm this? Is it 3.3v tolerant or does it need a voltage shifter?
  • Lastly, is there a schematic or pinout available for the arduino shield? I don't plan to use it on the end product but it will help with prototyping.

Thanks for any help! I have looked all over the verizon and avnet websites and found nothing. Even the link of the quick start card in the box (avnet.me/MonarchGo-Shield-GSG) seems to be dead. Very frustrating!

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 3 years ago in reply to TMS_Matt +1
    The documentation is available under NDA. I actually found AVNET's github examples for the Go more helpful than Monarch's docs. From my roadtest: More info on Avnet's Github: https://github.com…
  • TMS_Matt
    TMS_Matt over 3 years ago in reply to Jan Cumps +1
    Thanks, I guess I will have to take up the search with sequans. That was going to be my next step anyway but I figured I would see if I got anything on here... I can probably get the module connected with…
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to TMS_Matt +1
    I have experience with this unit with "not verizon" sim cards (2 different providers, in Europe, with every setting different from Verizon). It takes effort and changes in the AT commands - and in my case…
Parents
  • TMS_Matt
    TMS_Matt over 3 years ago

    OK, I finally found some useful documentation here:

    /products/devtools/avnetboardscommunity/monarch-go/m/files

    Which answers most of my questions about, however I am still looking for an AT reference. The uBlox one I have should work for generic commands but is there one for the Go module?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to TMS_Matt

    The documentation is available under NDA.

    I actually found AVNET's github examples for the Go more helpful than Monarch's docs.

    From my roadtest:

    More info on Avnet's Github: https://github.com/Avnet/sequans_python, and the corresponding post Sequans Monarch-Go Python Example .

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • TMS_Matt
    TMS_Matt over 3 years ago in reply to Jan Cumps

    Thanks, I guess I will have to take up the search with sequans. That was going to be my next step anyway but I figured I would see if I got anything on here... I can probably get the module connected with those examples, but I would really like a complete reference!

    If there are representatives from either company reading this: This is atrocious customer service. You advertise a turn key cellular device and then hide all the useful documentation. Why on earth would I need to sign an NDA for an AT command reference manual??? Most every other company has that linked on the product page of digikey! These aren't trade secrets, half of the AT commands are generic anyway! I shouldn't have to spend hours sleuthing and jumping through hoops just to get some data sheets!

    And then when I email avnet asking for the documents that are not only missing from their proper place: the *product page*, but also the dead link from the quick start card that came with the product. I get a canned email response along the lines of "we don't care enough to provide customer support for out products, we let our other customers take care of that for us, take it up with the forums". I'm not looking for 1 on 1 diagnosis, I just want some TM's and if they bothered to actually READ my email that would be obvious and they could have forwarded the requested documents!

    I am done with this rant, and I apologize for polluting the forum with it, I just hope that it may serve as a warning to anyone else considering integrating this product into one of their own. I can only imagine what kind of terrible support I would get if I had an actual technical issue! the ONLY reason I am stuck with this module is because my client is stuck on verizon and verizon feels it is beneath them to deliver SMS from devices using numbers from services such as Hologram . More scummy business practices from the corporate world... Otherwise I would be using the uBlox module that actually provides easy access to their documentation! 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to TMS_Matt

    Once you are over the rant Blush: it's actually a great product. As a modem, but also when you dig deeper and find that it has an embedded MQTT stack <3

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to TMS_Matt

    I have experience with this unit with "not verizon" sim cards (2 different providers, in Europe, with every setting different from Verizon). It takes effort and changes in the AT commands - and in my case a firmware upgrade of the Go (and an additional debugger to load that firmware that AVNET kindly shipped to me at no cost).

    If you are able to post your difficulties on the public forum here, I'll try to help.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to TMS_Matt

    I have experience with this unit with "not verizon" sim cards (2 different providers, in Europe, with every setting different from Verizon). It takes effort and changes in the AT commands - and in my case a firmware upgrade of the Go (and an additional debugger to load that firmware that AVNET kindly shipped to me at no cost).

    If you are able to post your difficulties on the public forum here, I'll try to help.