Return to the original Ultra96

Related Blog Posts
  • Porting PYQN to ZC702

    In this project we will port the PYNQ framework to the ZC702 development board.  Introduction The ZC702 is an official development board from Xilinx. This board sports a ZC7020 ZYNQ FPGA SoC. It comes with a number of peripherals including ...
  • Tips for Integrating WiFi on the Ultra96-V2

    A key feature of Avnet's Ultra96-V2 board is its WiFi and Bluetooth connectivity that is made possible using the on-board ATWILC3000 module from Microchip. This module is IEEE 802.11 b/g/n plus Bluetooth 5 LE and is certified in more than 75 countrie…
  • Infineon PMIC updates to Avnet products

    Over the past several months, we've seen situations arise on two of our platforms that ended up highlighting how nice it is to have some ability to "tweak" your on board power system. I've written two blogs in the past both referencing the programmab…