Ultra96 with Pynq and AWS Greengrass The Ultra96 is a development board built around the Xilinx Zynq UltraScale+ MPSoC to the Linaro96Boards specification. It includes dual-core ARM A53s, dual-core ARM R5s, 2GB of LPDDR4 memory, and an integrated FPGA fabric. The platform integrates with the PYNQ (Python + Zynq) framework and AWS Greengrass allowing for Python based IoT Edge applications to run in conjunction with high-speed deterministic applications on the heterogenous MPSoC compute platform.

image

 

Documentation and Supporting Information

 

Top

image

 

 

Related Blog Posts
  • Blog #3: Third Eye for Blind - How to Make and Modify a PYNQ Overlay

    In my second blog, I discussed the ZYNQ SoC and PYNQ overlay in detail. I also controlled the onboard LEDs of the Arty Z7 board with the onboard buttons and switches using the base overlay. At the beginning of this blog, I will show how I made a simp…
  • Blog #2: Third Eye for Blind - Deep Dive into ZYNQ & PYNQ

    This is my second blog for the Eye On Intelligence Challenge sponsored by AMD. In my first blog, I unboxed the challenger kit and prepared the Arty Z7 board for developing applications with Python. I will share my experience with the ZYNQ SoC and the…
  • Blog #1: Third Eye for Blind - Overview

    Introduction This will be my first blog post on the Eye On Intelligence Challenge. At the very beginning of my blog post, I would like to thank Element14 and the contest sponsor AMD for choosing me as one of the official challengers for the Eye On In…