EXPLORE-NFC
  • Products & Partners
  • Dev Tools
  • EXPLORE-NFC
  • More
  • Cancel
EXPLORE-NFC
Blog NFC What is it?
  • Blog
  • Forum
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join EXPLORE-NFC to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: mcb1
  • Date Created: 16 Feb 2015 4:30 AM Date Created
  • Views 1751 views
  • Likes 4 likes
  • Comments 3 comments
  • tag
  • explore-nfc
  • prox
  • nfc
  • transponder
  • micro_chip
Related
Recommended

NFC What is it?

mcb1
mcb1
16 Feb 2015

NFC stands for Near Field Communication

So what does that mean?. image

 

Below is a simplistic explanation of the term and some of the principles involved.

 

 

Radio Waves

Radio communication occurs because the voltage along an aerial wire, creates a magnetic field.

This field reacts with the earths magnetic field and as the changes occur so does the magnetic interference.

At the receiving end, this change in magnetic field induces a voltage on the aerial. The 'magic smoke' bits inside the receiver, convert this back to it's original form (more or less).

 

There is a non maths explanation here

http://www.antenna-theory.com/basics/whyantennasradiate.php

 

It can be refered to as EM or Electro Magnetic radiation but the true conversion doesn't occur until several wavelengths away from the source.

image

     Image source Near and far field - Wikipedia, the free encyclopedia

 

Within the near field reactive region, any conductive objects can cause the antenna can be detuned.

This is why the art of tuning antennas can be likened to ("non white magic" ... the correct term trips the blacklist ) (not NZ's America cup yacht) but the dark arts, since you can't see it, and often can't measure it, but the effect is there.

 

Somewhere along the line someone discovered that they could use this and the most common use is to pass small amounts of data.

 

 

 

NFC

I've never heard of it or used it. image

Until the later cellphones and credit cards with 'Tap and Go' the term NFC wasn't widely used.

 

I don't have one of those phones. image

Some people may have a Proximity Tag for access control into buildings, and these use the same principle.

imageimage

 



Don't work in one of those buildings. image

Anyone that has a modern car probably hasn't realised there is a tag inside their key, which is registered in the cars Engine Management Computer.

 

imageimageimageimage

    Image source  Google search various multiple finds




My car doesn't have one of those keys. image

If your pet is micro-chipped, they have a tag using the same technology inserted under the skin.

  imageimage

    Image source  Google search various multiple finds

 

No still not convinced I've used it. image

Well if you've ever been shopping you will have.

Many of the stores use security tags inside the products you buy.

While they may not contain data, they work on the principle of detuning the antenna at the shop entrance.


I don't have access to the technology they use (and it's not important here), but the reality is you will have experienced it somewhere.




So you may have using NFC technology for some time without realising it.

 

 

How does it work.

Contrary to popular belief the tags do not transmit. image

 

The reader sends out a signal at the designed frequency (usually 125 KHz, 134 KHz, 13.5 MHz) and when a tag is within range it captures that energy.

This provides sufficient energy to power the chip inside which then will short the antenna in a particular manner.

The shorted antenna will detune the readers antenna, resulting in a difference. (a shorted antenna acts like a large metal object)

The reader electronics will translate that pattern of 'shorts' and 'non-shorts' into data.

 

How the reader handles the resultant data depends on the design of the system.

 

These tags are referred to as 'passive', and for some inventory control an 'active' (powered) tag can be used.

 

 

 

Is it secure

That is a good question. image


It has been alleged that some credit cards used for 'tap and go' applications have shown that it may be possible to skim them, without the owner knowing.

(You can find various conspiracy theories on the internet ... they are all true) ...  image


In the past it required a physical swipe of the magnetic strip in order to collect the data, and you also needed a pin number, but with NFC unless there is a security handshake, the card/tag will give up its identity quite easily.

Some vendors have no pin required for transactions up to $80 ... meaning someone can do some damage to your account.

 

How can I protect myself. image

Since the card requires to be within a readers field, the application of metal either side of the card, renders it's performance extremely poor.

This has resulted in another industry for wallet protectors.

image

      image source Protect Your Credit Cards | Credit Card RFID Wallet - Full Sheild Protection

 

I've also heard of a piece of foil used inside your favourite wallet, but whatever is used, the idea is to prevent the tags getting a signal so it can respond.

 

 

Now that I've introduced you to what NFC is, the next blog will look at some of the uses, and how you can play with it.

 

 

Mark


edit

Next blog

NFC Uses

  • Sign in to reply
  • mcb1
    mcb1 over 11 years ago in reply to jw0752

    Thanks for that guys.

     

    Next blog is

    http://www.element14.com/community/community/designcenter/explorenfc/blog/2015/02/17/nfc-uses

     

    I'll edit the first one to show it.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 11 years ago

    Hi Mark,

    Thanks for shedding some light on this technology. I have added NFC to my list of electronic and site Initialisms.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago

    Hi Mark,

     

    Thank you for the great explanation, these are many questions I've asked myself too.

    This helps to explain some of the questions, facts and myths surrounding NFC.

    Looking forward to your next post on this topic!

     

    I'm also curious about who are the manufacturers/players in NFC space, and what technologies exist to

    run inventory on multiple items in one go (e.g. a box of items) - I heard this is possible (although might be some general

    RFID and maybe not NFC - not sure. Maybe an active tag gets used).