EXPLORE-NFC
  • Products
  • Dev Tools
  • EXPLORE-NFC
  • More
  • Cancel
EXPLORE-NFC
Forum card polling problem
  • Blog
  • Forum
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join EXPLORE-NFC to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 18 replies
  • Answers 2 answers
  • Subscribers 10 subscribers
  • Views 3053 views
  • Users 0 members are here
Related

card polling problem

Former Member
Former Member over 11 years ago

Hi

 

I have both the first raspberry pi and pi2. I am doing a college project and trying to make an NFC student registering system with the Pi and an explore-NFC add-on board. I have followed every single step from their start-up guide on trying the card_polling project demo but when I type ./card_polling to execute it, it just says:

/****** Begin Polling ******/

 

and stays like that without any further action.

Im using this on my new pi2.

 

Ive fully updated everything required as well! What am I doing wrong?

 

Thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • michaelneurohr
    michaelneurohr over 11 years ago +1 verified
    Hi, the software projects are not working anymore with the latest Raspbian image. Looks like the update is breaking something.
Parents
  • Former Member
    0 Former Member over 10 years ago

    The card-polling sample works on Raspbery Pi 2 with kernel 3.18, but there is a missing initialization after the line 329 of the file NxpRdLib_PublicRelease/comps/phbalReg/src/R_Pi_spi/phbalReg_R_Pi_spi.c :


    phStatus_t phbalReg_R_Pi_spi_Exchange(
    phbalReg_R_Pi_spi_DataParams_t * pDataParams,
    uint16_t wOption,
    uint8_t * pTxBuffer,
    uint16_t wTxLength,
    uint16_t wRxBufSize,
    uint8_t * pRxBuffer,
    uint16_t * pRxLength
    )
    {
    struct spi_ioc_transfer spi ;
    memset(&spi,0,sizeof(spi));   // add missing initialization


    Have a look at /usr/include/linux/spi/spidev.h to see that not all fields of spi_ioc_transfer are initialized.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago

    The card-polling sample works on Raspbery Pi 2 with kernel 3.18, but there is a missing initialization after the line 329 of the file NxpRdLib_PublicRelease/comps/phbalReg/src/R_Pi_spi/phbalReg_R_Pi_spi.c :


    phStatus_t phbalReg_R_Pi_spi_Exchange(
    phbalReg_R_Pi_spi_DataParams_t * pDataParams,
    uint16_t wOption,
    uint8_t * pTxBuffer,
    uint16_t wTxLength,
    uint16_t wRxBufSize,
    uint8_t * pRxBuffer,
    uint16_t * pRxLength
    )
    {
    struct spi_ioc_transfer spi ;
    memset(&spi,0,sizeof(spi));   // add missing initialization


    Have a look at /usr/include/linux/spi/spidev.h to see that not all fields of spi_ioc_transfer are initialized.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer