EXPLORE-NFC
  • Products & Partners
  • Dev Tools
  • EXPLORE-NFC
  • More
  • Cancel
EXPLORE-NFC
Forum Compile Examples
  • Blog
  • Forum
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join EXPLORE-NFC to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 15 replies
  • Subscribers 10 subscribers
  • Views 2755 views
  • Users 0 members are here
Related

Compile Examples

e14 Contributor
e14 Contributor over 11 years ago

Hello,

Firstly I would like to say sorry that I´m a very big noob at C programming, because I never did this before.

I had a look at the examples today and customised them a little bit. How do I compile the C files in order to run them now? I´m sure that cc -o basic basic.c is the wrong solution. I´m sure that the answer is very easy but as I´ve already mentioned I´m totally unexperienced with C, so please forgive me image

 

Thank you very much in advance.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelneurohr
    michaelneurohr over 11 years ago in reply to clem57 +1
    Hi Clem, the LPCXpresso IDE is only used for the software projects running on the MCUs LPC1769 and LPC1227. For the Raspberry Pi projects please build on the Raspberry Pi directly. Michael
  • e14 Contributor
    e14 Contributor over 11 years ago +1
    Of course. Firstly I´ve installed all libraries and extensions provided in the README.md file and afterwards I ran the following commands in the root folder of the source files: ./bootstrap ./configure…
Parents
  • michaelneurohr
    0 michaelneurohr over 11 years ago

    In the source files you should find a README file with step by step instructions about how to compile the sources.

    The easiest would be to compile directly on the Raspberry Pi. Otherwise you would need a cross toolchain.

     

    Let me know if that helps.

     

    Michael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to michaelneurohr

    HI Michael,

     

    can you give a brief explanation about cross compiling?

    Can it be done with Eclipse in Windows?
    I would love to debug apps there.

     

    Thanks a lot.

     

    Nikola

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to e14 Contributor

    If your compiler produces code that does not run on current machine, then you have a cross compiler. Yes, based on this Eclipse does this on Windows.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to clem57

    Thanks for a quick response Clem.
    Perhaps my question was too general and not specific.
    I did manage to cross compile a simple hello_world application.

    My concerns are how do I include the library in this environment?

    And which one: NXP NFC Reader Library or Neard?
    My idea is to develop a C NFC app using only NXP NFC Reader Library. What are my starting points?

     

    Nikola.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to clem57

    Thanks for a quick response Clem.
    Perhaps my question was too general and not specific.
    I did manage to cross compile a simple hello_world application.

    My concerns are how do I include the library in this environment?

    And which one: NXP NFC Reader Library or Neard?
    My idea is to develop a C NFC app using only NXP NFC Reader Library. What are my starting points?

     

    Nikola.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • clem57
    0 clem57 over 10 years ago in reply to e14 Contributor

    It would be better to open a new question then instead of hijacking this topic which is different.

    Clem