Dev Tools
  • Products
  • More
Dev Tools
Forum Decoupling capacitors behavior on power-off
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 84 subscribers
  • Views 1132 views
  • Users 0 members are here
Related

Decoupling capacitors behavior on power-off

modelrailwaycat
modelrailwaycat over 10 years ago

Hello,

 

I am designing a home control system which contains a 'net' of multiple PCBs. Each PCB has several decoupling capacitors, namely 1 large 100 uF capacitor near the power supply connector (5V), and several 100nF spread on the board close to the ICs Vcc pins (between 6 and 10 per board). The finished system will include about 60 boards like this, separated several centimeters or even meters one of each other, and all of them powered by the same power supply. So at the end all the capacitors will be paralelled to the power rails.

 

My question is about the behavior of the system when the power will be turned off. At this point, I realize I will have an equivalent +6000 uF capacitor. What should be considered regarding the design of the system or the power supply in order to guarantee a safe operation?

 

Thank you very much in advance!

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 10 years ago +1
    What should be considered regarding the design of the system or the power supply This is an excellent example of good engineering. The turn off shouldn't be much of an issue, as each board will draw…
Parents
  • mcb1
    mcb1 over 10 years ago

    What should be considered regarding the design of the system or the power supply

    This is an excellent example of good engineering.

     

    The turn off shouldn't be much of an issue, as each board will draw x current.

    You could check how long before the voltage drops to a level where the IC's stop working, and this would give you a time.

    One issue that can cause a problem is where a pin voltage exceeds the Supply voltage on the IC.

    (This can occur if the voltage is sourced from another part of the circuitry or interconnected boards.)

     

    With 60 boards using diodes in series with the supply becomes a logistical issue, but would ensure the spare energy in board X doesn't power board Y.

     

    I'd be more concerned with the Power On.

    6000uF is likely to represent a very high inrush of current, which could trip the supply or blow a fast acting fuse.

    You may wish to test the supply can handle the current peak when they all get powered on at once.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mcb1
    mcb1 over 10 years ago

    What should be considered regarding the design of the system or the power supply

    This is an excellent example of good engineering.

     

    The turn off shouldn't be much of an issue, as each board will draw x current.

    You could check how long before the voltage drops to a level where the IC's stop working, and this would give you a time.

    One issue that can cause a problem is where a pin voltage exceeds the Supply voltage on the IC.

    (This can occur if the voltage is sourced from another part of the circuitry or interconnected boards.)

     

    With 60 boards using diodes in series with the supply becomes a logistical issue, but would ensure the spare energy in board X doesn't power board Y.

     

    I'd be more concerned with the Power On.

    6000uF is likely to represent a very high inrush of current, which could trip the supply or blow a fast acting fuse.

    You may wish to test the supply can handle the current peak when they all get powered on at once.

     

    Mark