Dev Tools
  • Products
  • More
Dev Tools
Forum [How To] Mosfet switch for low forward voltage LEDs
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 79 subscribers
  • Views 987 views
  • Users 0 members are here
  • logic
  • lighting
  • led
  • Design
  • Technology
  • led_lighting
  • leds
  • power
Related

[How To] Mosfet switch for low forward voltage LEDs

Catwell
Catwell over 15 years ago
I had designed a transistor logic based switch for a LED based project recently at my day job. I discovered that the design I had, N-channel mosfet triggered by a PNP transistor, worked, but it didn't bring the voltage down far enough to turn off the LEDs I was working with. The LEDs in question had a forward voltage of 2.1V, but did they turn off after the voltage dropped below that? They did not. In fact, they would even be dimly lit as low as 1V. In other words, I was dealing with a situation where the LED's properties didn't follow the datasheet. You will always have a little voltage & current flowing through a transistor logic circuit, but I needed it clamped way down in this case.

 
I was in a bind, the project was due, I did what we all have to from time to time, pulled an all night design session. I ended up simplifying the overall design, made the final product cheaper, and brought the temperature down as well. I switch to a P-channel mosfet switch, bringing the "off" state voltage down to ~41mV. I then drew it up in Multisim, and the simulation worked perfectly. I had the PCBs  changed per my new design, and built 4 perfect prototypes.
 
Below I am showing a single case of the mosfet switch.

When "Line 1" is high/on, it will be cut off when "Line 2" is high. So that only LED2 will be on at that point.

R1 & R3 are resistors to limit the current for the LEDs.
The mosfet & diode are actual components I picked for the simulation. Final components I chose had similar properties.
image
If you have more LEDs or conditions, just replicate the setup for each.

 
 
I thought I would share this design for all those faced with a similar task.

 
Enjoy.

 
Cabe
  • Sign in to reply
  • Cancel
  • Catwell
    Catwell over 15 years ago

    I used this concept for a larger system full of complex logic.

     

    There was one case where if a line was high it should kill every other line. I placed the Mosfet switch setup on each line tied to the master.

     

    Cascading works fine. My initial voltage, on each line, was 12-14 so I wasn't worried about the drop across the diodes and mosfets affecting the required voltage at the LED. So, if you use this idea, be sure to account for the drop across each component headed towards each LED.

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down