Dev Tools
  • Products & Partners
  • More
Dev Tools
Forum MSP430 Graphical Peripheral Configuration Tool "GRACE"
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 79 subscribers
  • Views 4594 views
  • Users 0 members are here
  • grace
  • reference
  • design_tool
  • value_line
  • texas_instruments
  • mcu
  • msp430
  • launchpad
  • ti
Related

MSP430 Graphical Peripheral Configuration Tool "GRACE"

ssilberhorn
ssilberhorn over 15 years ago

FREE MSP430 Graphical Peripheral Configuration Tool "GRACE"


View View Grace Screenshot

 

- Fully harness MSP430 MCUs integrated analog and digital peripherals with Grace Software
Enable  and configure ADCs, DACs, timers, clocks, serial communication  interfaces and more, by interacting with buttons, drop-down menus, and  text fields. Navigate through the MSP430 MCUs highly integrated  peripheral set with ease.

 

- Grace software supports all MSP430F2xx and G2xx Value Line MCU devices
This means it supports the MSP430 MCUs most popular tools such as MSP-EXP430G2 LaunchPad, eZ430-F2013, eZ430-RF2500 and other tool kits.

 

- Seamless integration into TI's eclipse-based Code Composer Studio software
Grace software generates easy-to-understand C code, which is directly  inserted into your active project. This seamless integration into the integrated development  environment (IDE) allows the Grace generated code to be debugged and  downloaded into your MSP430 microcontroller just as if it was  handwritten.

Features
  • GUI-based configuration tool for setting up ADCs, OpAmps, Timers, Clocks,    GPIO, Comparators, Serial Communication, and other MSP430 peripherals.
  • Generates easy-to-understand C code that properly configures your device
  • Compatible with LaunchPad and most eZ430 tools
  • Grace tooltips offer helpful popups and hints for properly configuring    your MSP430 device
  • Grace provides a Basic, Power User, and Register-level view offering    different levels of abstraction for setting up your peripherals.
  • As a free CCS plug-in, Grace seamlessly integrates into the MSP430 tool    chain and development process
  • Minimizes any configuration conflicts or collisions between multiple    peripherals

Install Instructions:

Before installing the Grace product, please look over the Grace installation Wiki page at:  http://processors.wiki.ti.com/index.php/Grace_Installation

 

Download Instructions: click here

 

Related Information:

  • Grace Wiki Page: www.ti.com/gracewiki
  • Grace Getting Started Video - available from this tool folder
  • Grace    Feedback Forum
  • CCStudio Wiki: Support for CCS v4
  • Sign in to reply
  • Cancel

Top Replies

  • awinning
    awinning over 15 years ago +1
    Hi Shawn, Just watched the video and it looks a pretty clever piece of software. I've pasted the YouTube version below www.youtube.com/watch
Parents
  • Levas
    Levas over 4 years ago

    Information to everyone... TI abandoned graphical configuration tool. The only way to configure MSP430 is to read datasheets...  It hard, it is stupid. But  this is TI decision.

    I like STM32Cube idea, when not only init is created, but there is HAL and other libraries. It takes half hour to create some USB to something device without reading much of documentation.

    I wish that Grace could evolve to something better... but life is life.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Levas
    Levas over 4 years ago

    Information to everyone... TI abandoned graphical configuration tool. The only way to configure MSP430 is to read datasheets...  It hard, it is stupid. But  this is TI decision.

    I like STM32Cube idea, when not only init is created, but there is HAL and other libraries. It takes half hour to create some USB to something device without reading much of documentation.

    I wish that Grace could evolve to something better... but life is life.