Dev Tools
  • Products
  • More
Dev Tools
Forum Android 4.0.1 for x86 platforms, released
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 81 subscribers
  • Views 573 views
  • Users 0 members are here
  • android
  • pc
  • programming
  • knode
  • development
  • arm
  • multicore
  • x86
  • multi-cores
Related

Android 4.0.1 for x86 platforms, released

Catwell
Catwell over 14 years ago

image

The x86 version of Android 4 has been released for developers. This potentially brings the latest Android OS to billions of platforms. To developers out there, this sounds like a lucrative new market.

The tablets and cell phones with the OS on it have specifications that the PC market surpassed a decade ago, in many cases. Android can breathe new life into old systems.

At the moment, the x86 Android 4 has a few issues. Some sound functions, cameras, Ethernet, and Intel hardware acceleration does not have support, but AMD hardware, WiFi, and basics sounds do work. The source already has support for one PC tablet, the MSI Brazos Tablet. Get the source on Google's x86 porting page.

Try running Android 4 in a virtual box:
- Create a virtual machine, Linux (Virtual Box)
- Set memory size (1 GB)
- Create virtual harddrive
- Load the x86 Android ISO
- Install x86 Android
- In virtual box.. "Choose Create/Modify Partitions –> New –> Set as Primary –> set as Bootable –> choose Write, then you can format the new partition into ext3 filesystem."
- It ready
 
From Google Groups.

Cabe
http://twitter.com/Cabe_e14
  • Sign in to reply
  • Cancel
  • SGarciaV
    SGarciaV over 14 years ago

    No Ethernet? So if I understand correctly, I can install Android on my wired box, but I'll have no connectivity? If I want that I'll need Wifi? Is that correct? Thanks! Salvador

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Catwell
    Catwell over 14 years ago in reply to SGarciaV

    For now, the only Internet connectivity is via WiFi.

     

    I am sure Ethernet will be implemented soon.

     

    Cabe

    http://twitter.com/Cabe_e14
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • SGarciaV
    SGarciaV over 14 years ago in reply to Catwell

    Ok, thanks for the info. I'll wait till Ethernet support is available. I can install it on a Virtual Box machine, but would be nice to have connectivity. Salvador