Dev Tools
  • Products
  • More
Dev Tools
Forum How to troubleshoot a WI-PI
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 82 subscribers
  • Views 1801 views
  • Users 0 members are here
Related

How to troubleshoot a WI-PI

e14 Contributor
e14 Contributor over 13 years ago

Hey folks, my WI-PI only worked for one Day, I got it up and running yesterday, and today the blue LED wo'nt even light up. Can anyone suggest a troubleshooting method?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Another Wi-Pi installation problem!

     

    I followed the Wi-Pi installation manual and the Wi-Pi would not work at all. I made sure that I followed the instructions in the manual, I did the ping and received no connection. Then I thought I would check to see if the Wi-Pi would work on Windows 7. I plugged it into my PC and had it install the drivers but I could not get it to work there either.

     

    Then I checked the Advanced Settings for the Wi-Pi and basically enabled all that I could under that section. The Wi-Pi still would work no matter what I did even though I disabled the PC's wifi connection and plugged the Wi-Pi in again.

     

    Even though I could not get it to work on Windows, I though that this might have changed something internally for the Wi-Pi and plugged it into the RPi and booted it up. The ping was pinged, the Web worked and ta-da! Just to make sure that it was not a one-time thing, I shut down the RPi and restarted it with success.

     

    By the way, I could not get the ifconfig to come up before, when the Wi-Pi was not working, but it does come up now.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago

    Another Wi-Pi installation problem!

     

    I followed the Wi-Pi installation manual and the Wi-Pi would not work at all. I made sure that I followed the instructions in the manual, I did the ping and received no connection. Then I thought I would check to see if the Wi-Pi would work on Windows 7. I plugged it into my PC and had it install the drivers but I could not get it to work there either.

     

    Then I checked the Advanced Settings for the Wi-Pi and basically enabled all that I could under that section. The Wi-Pi still would work no matter what I did even though I disabled the PC's wifi connection and plugged the Wi-Pi in again.

     

    Even though I could not get it to work on Windows, I though that this might have changed something internally for the Wi-Pi and plugged it into the RPi and booted it up. The ping was pinged, the Web worked and ta-da! Just to make sure that it was not a one-time thing, I shut down the RPi and restarted it with success.

     

    By the way, I could not get the ifconfig to come up before, when the Wi-Pi was not working, but it does come up now.