Dev Tools
  • Products
  • More
Dev Tools
Forum Developing platform to final product options. Suggestions?
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 79 subscribers
  • Views 316 views
  • Users 0 members are here
  • microncontrollers
  • plc
  • i2c
  • input
  • sensors
  • io
  • output
  • spi
  • mcu
  • touchscreen
Related

Developing platform to final product options. Suggestions?

e14 Contributor
e14 Contributor over 13 years ago

Hi,

I am working on the developing a product that until now I had only considered an embedded PC or a PLC [C programmable] as possible final controllers.

I've been curious about the possibility of using a MCU or similar instead.

A little description of what I need to accomplish.

 

Analog Inputs = ~4 [so far]  [0 to 5V maybe 0 to 10V]

Analog Outputs = ~4 [so far] [0 to 5V maybe 0 to 10V]

Digital Inputs = ~ 5

Digital Outputs = 5~10 [so far] [possible PWM one or two - and relays]

Communication = RS232/485 and Ethernet mostly UDP for data/status sharing

Display = Touch screen 5 to 7"

 

Analog sampling doesn't need to be anything super fast. 1kHz is way more than I need. I might need some minor signal analisys [frequency detection]

The Ethernet communication would be mainly use to send and receive data from some legacy equipment and the touch screen for user interface [HMI]

 

Ideally I would love to find a controller that has all the I/O I need. I know that might not be the case, but as long as I can add it [I2C/SPI] fairly easy I think it might still work.

It would be nice if the processor comes with a developing board with diagrams so I can addapt the Optos[i/o] into one board.

 

It had been many years since I worked with any microcontroller [other than arduinos for a home project or two]. I can definitely benefit from a large community support [ARM/NXP/PIC/ETC]

 

I was hoping I could get some advice/suggestions to what I should look for or what boars to consider. I'll appreciate any information that I get.

 

Best,

 

Cristian