Dev Tools
  • Products
  • More
Dev Tools
Forum Windows Fun
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 81 subscribers
  • Views 801 views
  • Users 0 members are here
Related

Windows Fun

bprewit
bprewit over 13 years ago

I posted this on my blog, but I'm reposting it here so that everyone can see it.

 

Okay, I have said it before and I'll say it again .. I am *not* a windows user.  I used Win95 for a few weeks when it first came out (IIRC, I installed it from a stack of 3.5in disks), but then I moved into the *nix world and never went back.  For the last 15 years or so, if I had to have Windows to make it work then I sought another alternative.

 

Having said that, because so much of what we do here is Windows-only, I broke down and built a Windows computer.  My thought was "it's a tool for getting the job done" .. So I took an old Celeron system that I had laying around and installed XP Professional on it. After paying $79.00 or so for the OS then I had to install an anti-virus program.  (I used FreeAVG .. because it is free).  I'll admit it; I'm a cheapskate.  I'll help out in any way that I can, but I hate to spend money that I don't have to.   It is a constant source of amusement that people will accept buying an OS or a computer with a pre-installed OS, then having to purchase an additional product to keep the OS working ..


Since I've been a RedHat person for most of my career, I set up this computer to also boot Ubuntu 10.  The difference in performance between Windows and Ubuntu is amazing.  The old, dogged-out box that I had laying around, as I said, is a Celeron and was never top-of-the-line even when it was new.   Ubuntu on this system is never going to knock anybody's socks off but it is reasonably usable.

 

Not so usable with Window, unfortunately. I have been constantly frustrated with Windows since I set up the system.

 

I normally use RDP to access Windows from my MacBook.  This worked reasonably well unti today, when I could not log onto the Windows box.  Being the troubleshooting guru that I would like to think I am, I set out to determine what was keeping me from using RDP to access Windows.  Windows Firewall, disabled, check.  Ping the gateway from the windows box, check.  Ping the windows box, no-go.  Re-check windows firewall, disabled.  Ping google from the windows box, check.  Ping the windows box, no-go.  Re-check the settings on Windows firewall, still disabled.  Reboot the system, ping out OK but still can't ping the Windows box .. you get the idea.

 

Eventually, I discovered that a recent update to FreeAVG had installed *their own* windows firewall, and that was what was causing me grief.   Now, I do understand that Windows is full of security holes (never meant for the internet) and that a firewall is pretty indispensable in keeping the bad stuff off of your computer; but I have a router that handles the firewall so I don't really need another one on my internal LAN.  As soon as I disabled the FreeAVG firewall, things started working again.

 

And this brings me to the point of this essay:  Hey, FreeAVG, if you were going to firewall me out of business, couldn't you have told me?  For crying out loud, it took me nearly two hours to get back in business after the "upgrade" .. and I really hate having to troubleshoot my tools before I can troubleshoot my product!

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    johnbeetem over 13 years ago

    I have a Windows machine that I use for client projects and occasional software that doesn't run on GNU/Linux.  The way I keep it working is never, ever hook it up to the Internet image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 13 years ago in reply to johnbeetem

    Gents

    The IT guys at work put me onto Avast.

    Free and very little degrading of the computers performance.

     

    Beware the default time for checking for updates is not long enough and once a day is plenty.

     

    Personally I never use (nor recommend) Internet Explorer or Outlook and prefer to use Firefox and Thunderbird, so most of the security holes are gone.

     

    Windows seems to bog itself down with all the extra c%^*p running in the background, along with trying every different form of exploration of the network.

    If you run wireshark, you may be able to remove half of the traffic the Windows box generates that is not required.

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mcb1
    mcb1 over 13 years ago in reply to johnbeetem

    Gents

    The IT guys at work put me onto Avast.

    Free and very little degrading of the computers performance.

     

    Beware the default time for checking for updates is not long enough and once a day is plenty.

     

    Personally I never use (nor recommend) Internet Explorer or Outlook and prefer to use Firefox and Thunderbird, so most of the security holes are gone.

     

    Windows seems to bog itself down with all the extra c%^*p running in the background, along with trying every different form of exploration of the network.

    If you run wireshark, you may be able to remove half of the traffic the Windows box generates that is not required.

     

     

    Mark