Dev Tools
  • Products
  • More
Dev Tools
Forum XMOS giving away 2500 startKITs for FREE!
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 82 subscribers
  • Views 691 views
  • Users 0 members are here
Related

XMOS giving away 2500 startKITs for FREE!

xmos_support
xmos_support over 12 years ago

XMOS is running a 'HAPPY XMOS' campaign and is giving away 2500 startKITs to customers who sign-up and qualify, with boards shipping in time for the holiday season.

Chekout more inforamtion about startKIT. You can get your startKIT by registering here.

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to johnbeetem +1
    That is a good question. The connection is: Tile <-> JTAG <-> XTAG2 JTAG to USB key <-> gdb with libusb Arguably this could do with more user-facing documentation; but there is only finite time. Some links…
  • morgaine
    morgaine over 12 years ago +1
    Even more interesting than giving away 2500 startKITs for free is XMOS's other announcement of the moment -- "XMOS launches startKIT: multicore development for $14.99" . That's important, I think. Just…
  • johnbeetem
    johnbeetem over 12 years ago

    Very interesting device.  I have an application that might be suitable, so I took a look at some of the XMOS documentation.  One thing that was not immediately clear is whether it's possible to talk to the device directly over the debug interface, or do users have to run XMOS software on a host?  That is, is the format and content of the messages transferred over the USB debug interface documented?

     

    I think it's pretty nifty that startKIT can plug into RasPi.  It would be even niftier if RasPi could be used as the development platform with FLOSS tools.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to johnbeetem

    That is a good question.

     

    The connection is:

      Tile <-> JTAG <-> XTAG2 JTAG to USB key <-> gdb with libusb

    Arguably this could do with more user-facing documentation; but there is only finite time.

     

    Some links that may be helpful

     

    * A (slightly dated) version of the XTAG2 software is on-line: https://github.com/xcore/sc_jtag/tree/master/module_xcore_debug/src, and https://github.com/xcore/proj_xtag2/tree/master/app_l1_jtag

    These two together should enable you to work out the protocol on both USB and JTAG.

     

    * https://www.xmos.com/en/download/public/Dynamic-code-loader-for-XTAG2.pdf shows how to run other things on an XTAG2.

     

    You can also boot it over SPI; the format of the raw SPI image is documented in the datasheet of the devices.

     

    Hope this helps

    Henk

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago

    Even more interesting than giving away 2500 startKITs for free is XMOS's other announcement of the moment -- "XMOS launches startKIT: multicore development for $14.99".  That's important, I think.

     

    Just 2500 units won't go far, but making the basic evaluation kit just $14.99 puts it right alongside the microcontroller kits released by the big boys like ST, TI, Freescale and others.  Because that kind of money is well below the radar for practically everybody including most youngsters, it could lead to an awful lot of XMOS kit in circulation.  That's very good for company exposure, much better than hiring a PR company for promotion which is a one-shot waste.