Dev Tools
  • Products
  • More
Dev Tools
Forum Missing libraries for PinChangeInterrupt
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 79 subscribers
  • Views 440 views
  • Users 0 members are here
Related

Missing libraries for PinChangeInterrupt

e14 Contributor
e14 Contributor over 12 years ago

Hi,

I have this simple program to test from scratch and it fails to compile. I get these meesages:


G:\GV\Elektronika\Arduino\arduino-1.0.5-r2\libraries\PinChangeInterrupt\PinChangeInterrupt.cpp:50: error: 'NUMBER_PIN_CHANGE_INTERRUPT_HANDLERS' was not declared in this scope

G:\GV\Elektronika\Arduino\arduino-1.0.5-r2\libraries\PinChangeInterrupt\PinChangeInterrupt.cpp: In function 'void attachPcInterrupt(uint8_t, void (*)(), uint8_t)':

and so on ...

 

When I look into PinChangeInterrupt.h I see that there are few libraries refered to. Namely, inttype.h and core_build_options.h. I believe they might be causing problem. I looked through Arduino IDE 1.0.5 directories and can find inttype.h in \arduino-1.0.5-r2\hardware\tools\avr\avr\include (can not find core_build_options.h though). Shall I put  inttypes.h into \arduino-1.0.5-r2\libraries or am I having some other problem?


#include <PinChangeInterrupt.h>

 

void setup()

{

  pinMode(A0, INPUT);    // Pin A0 is input to which a switch is connected

  pinMode(A1, INPUT);    // Pin A1 is input to which a switch is connected

  pinMode(A2, INPUT);    // Pin A2 is input to which a switch is connected

    attachPcInterrupt(3,pressButton,RISING);

}

 

void loop() {

  /* Nothing to do */

} 

 

void pressButton()

{           // Interrupt service routine. Every single PCINT8..14 (=ADC0..5) change

            // will generate an interrupt: but this will always be the same interrupt routine

  if (digitalRead(A0)==0)  ;

  if (digitalRead(A1)==0)  ;

  if (digitalRead(A2)==0)  int aaa=1;

}