Dev Tools
  • Products
  • More
Dev Tools
Forum Question on wireless technologies
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 83 subscribers
  • Views 764 views
  • Users 0 members are here
  • internet_of_things
  • nrf
  • wireless
  • home_and_building_automation
Related

Question on wireless technologies

vish
vish over 12 years ago

Hi element14,

 

As a part of my hobby project, I want to implement some wireless communication between my modules. When I went scouting for the parts, I became confused.

I previously know about WiFi, Bluetooth and ZigBee. But now I'm started seeing some thing called 2.4GHz modules, but can't figure out what exactly this means.

Also I saw nRF24xxx in some posts. How is this different?

What would you suggest if I want to have a data rate of minimum  200KBPS in say some 12m radius with some 4-6 walls in between? I will have some 8-12 nodes in my network that needs to be connected.

 

Thanks ahead,

vish

  • Sign in to reply
  • Cancel
  • lrubanka
    lrubanka over 12 years ago

    Hi Vish,

     

    The 2.4GHz frequency range is an unlicensed area used by all sorts of different radio technologies.  As you mention, Wifi, Zigbee, 802.15.4 (underlies Zigbee), and lots more.  There are other unlicensed areas in the radio spectrum.  You can find out more with your favourite search engine.

     

    Have a look at the Open Energy Monitor project.  You'll find details about some wireless chips/modules they use.  Also have a look at the TI CC1101.  It's my personal favourite.  Nordic semiconductor nrf24l01 modules.

     

    One final recommendation, PanStamp.  It is a Atmega or MSP430 based wireless radio and microcontroller system with an excellent protocol for sensor and actuator networks.  PanStamp supports web integration and interoperability with a variety of popular tools.  It's all open source, and the creator sells nice hardware modules too.

     

    Good luck,

    Lawrence

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 12 years ago

    Lower frequencies penetrate walls better, so look for lower frequency radios. (433 MHz will penetrate better than 2.4 GHz)

    To get through 6 walls will likely require more power than a typical unlicensed radio module will provide. Bluetooth Class 1 is rated to go 100 m. I have run it through 6 walls but you may still have trouble with 6 walls, depending on what they are made of.

    You may need to resort to directional antennas, so choose radios that allow an external antenna to be substituted.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • waelect
    waelect over 12 years ago

    I noticed your tag as Internet of Things, If that is more relevant then WiFi will be your best bet.

     

    Lower frequencies have a better chance of getting through walls but require longer antennas, so if you project doesn't matter in regards to size then lower frequencies are a good alternative. The major downside to lower frequencies though is data throughput is way lower than 2.4GHz.

     

    At 200 Kbps you will be running close to the ceiling of 433MHz so your best bet would be 2.4GHz

     

    There is also 315MHz, 868-915MHz, the higher the frequency the faster the data rate, as the bandwidth is higher at these frequencies

     

    Malcolm

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • electronichamsters
    electronichamsters over 12 years ago

    Hello Vishnu,

    Are you using Arduinos by any chance?

     

    For wireless transceivers, my favorite is the RFM69HW, followed by the nRF24L01...as long as you have the freedom to define your protocol.  If you simply want to have two Arduinos talking wirelessly to each other, these are the best and cheapest, with the most flexibility.  I recommend taking a look at the RFM69HW.  It's not as well known as the nRF24L01, but it's got much better range (over 700 feet through walls).  Both are capable of encryption and sleep, so they work well for battery powered Arduinos.

     

    The RFM69HW is $4 each, the nRF24L01+ (high power version) is about $6.  The only disadvantage to the RFM69HW is that it's not 5V tolerant, but I've pretty much transitioned all my Arduinos to 3.3V.  Edit:  also wanted to add that RFM69HW is 915MHz, and nRF24L01+ is 2.4GHz.

     

    I use them extensively in my budding home automation project.  I don't like zigbee or bluetooth because they're expensive...if you want lots of nodes, the cost adds up.  Plus they don't have as good a range.

     

    Inexpensive & Flexible Home Automation / Wireless Sensors

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to electronichamsters

    The other option is Nordic NRF905 which can do 433, 868, 915 MHz

    There are libraries around and are similar to the 2.4Ghz versions, although not quite as cheap.

     

     

    Mark