Dev Tools
  • Products & Partners
  • More
Dev Tools
Forum I sorely need help driving two MOSFETs
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 14 replies
  • Answers 1 answer
  • Subscribers 82 subscribers
  • Views 3342 views
  • Users 0 members are here
  • driver
  • mosfet
  • q-switch
  • frontpage
  • p-channel
  • rf
  • n-channel
Related

I sorely need help driving two MOSFETs

e14 Contributor
e14 Contributor over 11 years ago

I've never used MOSFET drivers before and I've been bamboozled by the advice that is out there to the point that I don't know what's happening anymore!

 

I've attached a diagram of my circuit: the N-Channel MOSFET is a STP15N95K5 and the P-Channel is a IXTX32P60P. Its purpose is to turn on/off coupling between the transformer windings such that energy can be taken out of the driven, resonant side and dump to ground.

 

This is what I want:

TTL inputN-Channel Gate potentialP-Channel Gate potential
0.0 V ≤ 0.0 V ≥ 0.0 V
3.3 V+12.0 V-12.0 V

 

In operation to the TTL will normally be low but will high for a few microseconds after a strong (hundreds of volts) RF pulse on the driven side of the transformer. Ideally the MOSFETs should open as quickly as possible but shut gently.

 

At the moment I am doing something weird and unorthodox with op amps but the circuit is destroying them and I concede it was a bad idea.

 

I would be extremely grateful for any advice in terms of control circuit design (especially MOSFET driver recommendations) and please understand I'm not really au fait with MOSFETs!

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 11 years ago in reply to shabaz +1
    I can't find any information on Q-switching related to resonant circuits If I recall my days in RF, it could be referring to this, but I don't recall it being referred to as Q switching. (However my…
  • shabaz
    shabaz over 11 years ago in reply to mcb1 +1
    Hi Mark, That's a good reference to the amplifier classes, very interesting read. I too don't remember anything RF related being known as Q-switching - but my memory level is low too! Also the use of op…
Parents
  • shabaz
    0 shabaz over 11 years ago

    I'm not surprised if you've had confusing advice, perhaps some people have not understood the circuit.

    Neither do I I'm afraid. It can't turn on / off coupling unless you physically could move the windings (perhaps with a motor).

    By 'dump to ground' do you mean place a load across the transformer? (If not, please clarify - 'dump to ground' is not an

    electrical engineering term I've ever heard of).

    If you mean to place a load, then since your output is rectified (I notice you have a bridge rectifier there) you only need a single

    MOSFET to place a load (i.e. a very small resistance) across the rectified output. It wouldn't require the dual MOSFET

    arrangement (which then brings up more questions about why the dual op-amps and dual MOSFETs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to shabaz

    Hi shabaz, thanks for your reply and you're right, I could be clearer in what I mean.

     

    Essentially this is a circuit known as a Q-switch. Following a large RF signal on the resonant circuit the system experience what is known as "ringing", where despite not being driven the coil still emits RF as there is energy stored in the inductance/capacitance. By "dump to ground" I was just trying to emphasise that the MOSFET side of the circuit doesn't do anything except give the secondary wingings a route to ground. When there is a path to ground then the induced voltage can flow to ground and energy is taken out of the oscillating system.

     

    Does that make more sense?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 11 years ago in reply to e14 Contributor

    Hi Nick,

     

    I can't find any information on Q-switching related to resonant circuits. I can find information related to lasers.

    Do you have a link to a book/journal explaining it? (Not an internet page - there is a lot of junk out there - I want

    something written by an engineer and peer reviewed for a reputable journal).

     

    Anyway, if you want to perform switching to a load at any point then it doesn't need two MOSFETs as mentioned earlier - just

    use a single one (N-ch) and you can apply your 3.3V logic signal to the gate through a small resistor.

    That's a first approximation, anything more may need hiring an engineer to help you with specifics and run measurements for

    you, etc.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 11 years ago in reply to shabaz

    I can't find any information on Q-switching related to resonant circuits

    If I recall my days in RF, it could be referring to this, but I don't recall it being referred to as Q switching.  (However my recall is sometimes less than 10%  image)

    Amplifier Classes C to H

     

    The transmitter/amplifier relies on the Q of the resonant circuit to provide the rest of the waveform.

     

    mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 11 years ago in reply to mcb1

    Hi Mark,

     

    That's a good reference to the amplifier classes, very interesting read.

    I too don't remember anything RF related being known as Q-switching - but my memory level is low too!

    Also the use of op-amps and the reference to 2.5MHz and 'ttl' levels of 3.3V makes it hard to figure out the actual requirements and intent unfortunately : (

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to shabaz

    Best to ignore the op amp idea - as I said, it wasn't a good one.

     

    If you're willing to read a short paper here is one that I am basing elements of my work on [Dropbox download]

    "Suppression of Transient Processes in the Oscillatory Circuit of the NQR Spectrometer" - Rudakov (2000)

     

    The reason there are two MOSFETs is so that both halves of the rectified RF have a route to ground.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to mcb1

    Hi Mark, thanks for your response but this isn't the application I was thinking of. Q-switching is a term that gets used in NMR / MRI circles referring to changing the quality factor of a resonant circuit (RF coil). For more detail please see the paper I've linked in a reply to shabaz!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to mcb1

    Hi Mark, thanks for your response but this isn't the application I was thinking of. Q-switching is a term that gets used in NMR / MRI circles referring to changing the quality factor of a resonant circuit (RF coil). For more detail please see the paper I've linked in a reply to shabaz!