Dev Tools
  • Products
  • More
Dev Tools
Forum I sorely need help driving two MOSFETs
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 14 replies
  • Answers 1 answer
  • Subscribers 82 subscribers
  • Views 3299 views
  • Users 0 members are here
  • driver
  • mosfet
  • q-switch
  • frontpage
  • p-channel
  • rf
  • n-channel
Related

I sorely need help driving two MOSFETs

e14 Contributor
e14 Contributor over 11 years ago

I've never used MOSFET drivers before and I've been bamboozled by the advice that is out there to the point that I don't know what's happening anymore!

 

I've attached a diagram of my circuit: the N-Channel MOSFET is a STP15N95K5 and the P-Channel is a IXTX32P60P. Its purpose is to turn on/off coupling between the transformer windings such that energy can be taken out of the driven, resonant side and dump to ground.

 

This is what I want:

TTL inputN-Channel Gate potentialP-Channel Gate potential
0.0 V ≤ 0.0 V ≥ 0.0 V
3.3 V+12.0 V-12.0 V

 

In operation to the TTL will normally be low but will high for a few microseconds after a strong (hundreds of volts) RF pulse on the driven side of the transformer. Ideally the MOSFETs should open as quickly as possible but shut gently.

 

At the moment I am doing something weird and unorthodox with op amps but the circuit is destroying them and I concede it was a bad idea.

 

I would be extremely grateful for any advice in terms of control circuit design (especially MOSFET driver recommendations) and please understand I'm not really au fait with MOSFETs!

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 11 years ago in reply to shabaz +1
    I can't find any information on Q-switching related to resonant circuits If I recall my days in RF, it could be referring to this, but I don't recall it being referred to as Q switching. (However my…
  • shabaz
    shabaz over 11 years ago in reply to mcb1 +1
    Hi Mark, That's a good reference to the amplifier classes, very interesting read. I too don't remember anything RF related being known as Q-switching - but my memory level is low too! Also the use of op…
Parents
  • peterjcs23
    0 peterjcs23 over 11 years ago

    For the P channel mosfet you could use LTC1693-5; it has a power supply range of 4.5 to 13v and needs a high input of at least 3.1V

    And for the N channel the equivalent part is LTC1693-1.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • peterjcs23
    0 peterjcs23 over 11 years ago

    For the P channel mosfet you could use LTC1693-5; it has a power supply range of 4.5 to 13v and needs a high input of at least 3.1V

    And for the N channel the equivalent part is LTC1693-1.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to peterjcs23

    Hi peterjcs23

     

    Thank you very much for your suggestions. One question about the driver for the P-channel - shouldn't it output a negative drive voltage? Or have I got the wrong end of the stick?

     

    Nick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • peterjcs23
    0 peterjcs23 over 11 years ago in reply to e14 Contributor

    I understand the chip does the level shifting for you. It also has a pin that allows you to select the sense of the output. I would suggest you go on the Linear Technology site and get samples to try it out.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to peterjcs23

    Excellent, thanks again I really appreciate it!