Dev Tools
  • Products
  • More
Dev Tools
Forum How do I raise an input event using Pi face 2 on the Raspberry Pi 2 ?
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 81 subscribers
  • Views 643 views
  • Users 0 members are here
  • ras_pi
  • piface
Related

How do I raise an input event using Pi face 2 on the Raspberry Pi 2 ?

e14 Contributor
e14 Contributor over 10 years ago

Do I have to scan the inputs and catch the input on a scan or is there an event that I can raise when an input is received ?  I am using the MCP23S17 and PiFaceDigital2 classes that Peter Oakes demonstrated at https://www.youtube.com/watch?v=GaB4uUzv6w4

 

In the demo Peter used an item from the UI to catch inputs (i.e. LED0)  If anyone has put the library to use in a C# application and is very familiar with it, please reach out to me and lets discuss some training image

  • Sign in to reply
  • Cancel
  • bobalexander
    0 bobalexander over 10 years ago

    To my knowledge, you must continuously scan the inputs.

    That said, you should be able to write either a separate program or possibly a separate thread to do what you want.

    This is the event listener I have been using (in Python):

    Reference — PiFace Digital I/O 3.0.5 documentation

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gdstew
    0 gdstew over 10 years ago in reply to bobalexander

    Section 6 (pg. 89) of the data sheet on the BCM2835 shows that interrupts can be generated on any GPIO pin by logic level or a rising or falling edge on the pin

    when it is configured to be an input. The registers needed to do that are also described in that section however I do not know if it is supported by any existing

    I/O pin port access software and if it is not, writing the interrupt handler would be the biggest challenge.

     

    Edited to add:

     

    Link to BCM2835 data sheet:

     

    Broadcom: Datasheet for BCM2835 ARM Peripherals