Dev Tools
  • Products
  • More
Dev Tools
Forum Security camera project
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 81 subscribers
  • Views 1602 views
  • Users 0 members are here
  • camera.
  • frontpage
  • security_camera
Related

Security camera project

e14 Contributor
e14 Contributor over 10 years ago

Hi.

I have 30 years experience in PC software development but limited experience with embedded systems. I have a little experience with PIC using GSM modems.

I am researching components that are best suited for creating a security camera with the following capabilities.Ethernet/wifi and GSM communication, Must be able to run a web browser and be ONVIF compliant.

It must have inputs and outputs. Must be able to receive wireless remote comms to arm and disarm the system.

The camera must have motion detection and night vision.

I am looking at the raspberry pi, but to me it seems like a generic PC and not designed for any specific application.

There are a number of security cameras on the market that perform 80% of the tasks that I require, and I would hate to reinvent the wheel.

So if there is a standard camera board out there that does most of what I need with hooks to complete the project, it will be first prize.

Any help in this regard will be greatly appreciated.

  • Sign in to reply
  • Cancel

Top Replies

  • DAB
    DAB over 10 years ago +1
    Depending upon frame rates, an RPI with the NOIR camera running OpenCV could probably do the job. OpenCV has motion detection algorithms and the NOIR captures near IR between .8 and 1.2 microns. You could…
  • e14 Contributor
    e14 Contributor over 10 years ago +1 suggested
    I think Using a RPI for that purpose would be not only an ineffective overkill, but also a waste of effort. Most of the security cameras in the market perform all of the tasks you need for prices starting…
Parents
  • DAB
    0 DAB over 10 years ago

    Depending upon frame rates, an RPI with the NOIR camera running OpenCV could probably do the job.

     

    OpenCV has motion detection algorithms and the NOIR captures near IR between .8 and 1.2 microns.

     

    You could also probably use a PC or laptop with a NOIR camera and find application software that can implement the functions you want, either on the web or on the PC.

     

    Lots of options exist.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to DAB

    Thanks for the quick response DAB.

    Once a prototype has been developed on an RPI, should a scaled down version of the board be designed for mass production?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to DAB

    Thanks for the quick response DAB.

    Once a prototype has been developed on an RPI, should a scaled down version of the board be designed for mass production?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • DAB
    0 DAB over 10 years ago in reply to e14 Contributor

    Hi Clive,

     

    You need to do a lot of market research to determine what your cost/benefit space looks like.

     

    I am not sure that you can create a sustainable product using the RPI, but you can look at the issues once you establish your base cost and capabilities.

     

    I can only tell you that it is feasible.  The issues of a viable product are outside my experience base.

     

    DAB