Dev Tools
  • Products & Partners
  • More
Dev Tools
Forum Series RC circuits in parallel
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Answers 3 answers
  • Subscribers 82 subscribers
  • Views 4752 views
  • Users 0 members are here
  • rc circuits
  • mathematics
  • equivalent circuits
Related

Series RC circuits in parallel

e14 Contributor
e14 Contributor over 9 years ago

Morning all, happy new year!

 

Mathematical query today, one of simplification:

 

The circuit

image

Here we have a parallel circuit of two identical series RC circuits.  I.E. both resistors are identical and both caps are identical (this is key).

 

The question:

What is the equivalent circuit as a single series RC circuit.  I.E. what are the equivalent resistor and cap values?

image

I'm certain there is a solution to this when the parallel circuits are identical.  I'm aware that if they weren't there would be oscillation etc, but this isn't relevant in this case...in a way it is just two high ESR caps in parallel.

 

Many thanks

 

Simon

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 9 years ago in reply to jc2048 +4
    That's positively evil.
  • rachaelp
    rachaelp over 9 years ago +3 verified
    Hi Simon, It's exactly like two caps in parallel regardless of their ESR as all caps still have some resistance, even low ESR ones, so this is just what you would see with any bulk decoupling caps in parallel…
  • jc2048
    jc2048 over 9 years ago +3 suggested
    Rats! A Champion got there before me. My answer was going to be this (I'll post it anyway because it's a different approach): If the two sides are identical, the voltages at the nodes between the resistors…
Parents
  • mcb1
    0 mcb1 over 9 years ago

    My immediate thought is that any ripple on the VCC line will have two (identical) paths to go.

    Since they are the same values, then it must be half the 'impedance'.

    So the equivalent resistance will be half while caps in parallel double.

     

    My punt is (without resorting to google) that R is half and C is twice.

     

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 9 years ago

    My immediate thought is that any ripple on the VCC line will have two (identical) paths to go.

    Since they are the same values, then it must be half the 'impedance'.

    So the equivalent resistance will be half while caps in parallel double.

     

    My punt is (without resorting to google) that R is half and C is twice.

     

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer