Dev Tools
  • Products & Partners
  • More
Dev Tools
Forum Personal Project electrical question
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 2 replies
  • Answers 2 answers
  • Subscribers 79 subscribers
  • Views 974 views
  • Users 0 members are here
  • electrical
  • dc
  • video games
Related

Personal Project electrical question

alanwarrick
alanwarrick over 9 years ago

Hello all,

 

I am new here. I have a personal project here for the sake of brevity ill refer to as NX Harbor.

 

I have some electrical challenges, there are two major components to this projects that will require a fair bit of power at different draws.

 

One component's supply is listed as a 12v4a(48w) supply, i know for a fact it will not use this much power as it is a generic supply and the important number is the 12v

 

the second one is the challenge, i know for a fact that this device at most uses 15v@1.2a typically at peak.

 

The challenge here is that i want to power both of these off of a single battery bank with between 3-4Ah capacity and is no more than an inch thick.

 

I hope this is a no brainer for someone out there somewhere, and to you, thank you in advance.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 9 years ago +4 suggested
    Hi Alan, shabaz has given you some great ideas. One other thing that would be a good idea is to use an ammeter to get a real world measurement of the current draw of each of the two devices. One other…
  • shabaz
    shabaz over 9 years ago +3 suggested
    Hi Alan, Unfortunately there isn't enough information (battery capacity cannot be deduced from an Ah value, unless you specify the voltage of the battery bank; a 1.2V 3AH battery can store ten times less…
Parents
  • jw0752
    0 jw0752 over 9 years ago

    Hi Alan,

     

    shabaz  has given you some great ideas. One other thing that would be a good idea is to use an ammeter to get a real world measurement of the current draw of each of the two devices. One other thing to think about is that depending on what type of device we are talking about you may find that the 12 volt device can tolerate 13.5 volts and the 15 volt device can also tolerate 13.5 volts. If they will operate satisfactorily at 13.5 volts you are back to a one voltage solution which might be easier as this is very close to (2) Lithium  or (2) NiMH battery packs in series.

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 9 years ago

    Hi Alan,

     

    shabaz  has given you some great ideas. One other thing that would be a good idea is to use an ammeter to get a real world measurement of the current draw of each of the two devices. One other thing to think about is that depending on what type of device we are talking about you may find that the 12 volt device can tolerate 13.5 volts and the 15 volt device can also tolerate 13.5 volts. If they will operate satisfactorily at 13.5 volts you are back to a one voltage solution which might be easier as this is very close to (2) Lithium  or (2) NiMH battery packs in series.

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer