Dev Tools
  • Products & Partners
  • More
Dev Tools
Forum Thermal Dynamic of foam?
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 5 answers
  • Subscribers 80 subscribers
  • Views 4282 views
  • Users 0 members are here
Related

Thermal Dynamic of foam?

colporteur
colporteur over 6 years ago

When did foam become a good thermal conductor?

 

I studied electronics when Marconi was developing wireless technology. Well maybe not that far back. My career started on the cusp of the transition from glass transistors to semiconductor transistors. The one course in technical school that I had to pass and stood in the way of me graduating from college was Thermal Dynamics, the design consideration for heat transfer in the electronic components. The instructor was an Engineer and the Dean. I found him a poor instructor and struggled in the course. Our relationship deteriorated the more I struggled. I did mange to graduate. The Dean signed off on my thesis paper to graduate.

 

I recall it was important to span the air gap between a component and the heat sink. Sizing the heat sink was important but that air gap left unaddressed impacted the design. Liquid thermal compound we called paste was the go to solution. It filled the air gap to increased the thermal conductivity between the components and heat sink. About ten years ago I came across a thermal tape to replace the thermal paste. It was cleaner. Now I discover a foam?

 

image

 

I purchased a knock-off Pi4B metal case that doubles as a heat sink. The air gap between the Pi components and the metal case was close to a 16 of an inch. Wow! Included in the kit was foam pads. More pads (red circle) than required to cover the components that needed a heat sink. I was sceptical it would worked. Using the stress test posted here https://core-electronics.com.au/tutorials/stress-testing-your-raspberry-pi.html I discovered the metal case warms up but Hey it works.

 

My question to those individuals that never heard of a glass transistor, meaning your learning is newer than mine, on a scale of best to worse thermal conductivity solutions what is used today for bridging the thermal gap?

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 6 years ago in reply to shabaz +4 suggested
    I purchased a fitting SIL pad for the heat sink that I'm using for my electronic load. It's perfectly matching the flat contact part of the sink. It's less messy to apply compared to paste. Like double…
  • fmilburn
    fmilburn over 6 years ago +3 suggested
    I have worked extensively with heat transfer but not in the context of electronics. Curious, I looked at what Newark offers. They list 224 different products that can be sorted by thermal conductivity…
  • shabaz
    shabaz over 6 years ago +3 suggested
    Hi Sean, I've seen 'SIL-pads', those are available in different thicknesses (up to about 4mm) and are squishy but spread out, so are more like very soft rubber in feel, and don't feel like they have an…
Parents
  • shabaz
    0 shabaz over 6 years ago

    Hi Sean,

     

    I've seen 'SIL-pads', those are available in different thicknesses (up to about 4mm) and are squishy but spread out, so are more like very soft rubber in feel, and don't feel like they have an air foam. (EDIT - got the name wrong.. GAP PAD is a brand name for the thicker more squishy ones. Other manufacturers have different names for similar stuff).

    Those are the more orthodox way of handling varying air gaps, but I guess foam may work to an extent.

    My Pi 4 is in a large plastic case and has no heatsink (I don't do much processing with it), and the case gets warm, through conduction through the PCB and so on. I've not got around to finding a heatsink for it yet, and due to the particular enclosure I'm using I might need a fan eventually : (

    However for now (with the light processing) it's been running non-stop for weeks as-is, so I'm only going to attach the fan as a last resort.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 6 years ago

    Hi Sean,

     

    I've seen 'SIL-pads', those are available in different thicknesses (up to about 4mm) and are squishy but spread out, so are more like very soft rubber in feel, and don't feel like they have an air foam. (EDIT - got the name wrong.. GAP PAD is a brand name for the thicker more squishy ones. Other manufacturers have different names for similar stuff).

    Those are the more orthodox way of handling varying air gaps, but I guess foam may work to an extent.

    My Pi 4 is in a large plastic case and has no heatsink (I don't do much processing with it), and the case gets warm, through conduction through the PCB and so on. I've not got around to finding a heatsink for it yet, and due to the particular enclosure I'm using I might need a fan eventually : (

    However for now (with the light processing) it's been running non-stop for weeks as-is, so I'm only going to attach the fan as a last resort.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to shabaz

    I purchased a fitting SIL pad for the heat sink that I'm using for my electronic load. It's perfectly matching the flat contact part of the sink.

    It's less messy to apply compared to paste. Like double-sided tape.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer