Dev Tools
  • Products & Partners
  • More
Dev Tools
Forum Hack old vending machine touch pad to control LED lights
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 4 answers
  • Subscribers 82 subscribers
  • Views 4779 views
  • Users 0 members are here
  • touchpad
  • vending_machines
  • led controller
  • led lighting technology
Related

Hack old vending machine touch pad to control LED lights

goatyhead
goatyhead over 6 years ago

I am converting an old vending machine into a box you can sit in and i wanted to hack the vending machine touch pad to be able to change the lighting patterns of LED strips i want to mount inside the box.  the touch pad has 21 buttons, and a 12 pin attachment.  (i attached a photo of it).  I am  a newbie at electronics and it was hard to even find a place to ask a question like this.  Any help will be appreciated.

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 6 years ago +5 suggested
    Mike, These switches are usually connected as a matrix of rows and columns, with the switches connected between them. Like this: Using an ohm meter, connected between a column and a row, press the switches…
  • dougw
    dougw over 6 years ago in reply to goatyhead +4 suggested
    No power needed - the resistance meter has its own power. It is not a good idea to measure resistance with power on the controller as it can overload the meter.
  • goatyhead
    goatyhead over 6 years ago in reply to genebren +2
    that's a great start. For the Ohm meter to work, do i need to connect the controller to a power source? so, ill need a power supply (transformer). This will connect to some sort of receiver. The receiver…
Parents
  • genebren
    0 genebren over 6 years ago

    Mike,

     

    These switches are usually connected as a matrix of rows and columns, with the switches connected between them.  Like this:

    imageimage

    Using an ohm meter, connected between a column and a row, press the switches until you see a low ohm reading.  Just guessing from the image of the pad/connector, that the three pins towards the right might be the columns and 7 or the 8 pins to the left might be the rows.

     

    Hopefully this will help you get started.

    Good Luck!

     

    Gene

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • goatyhead
    0 goatyhead over 6 years ago in reply to genebren

    that's a great start. 

     

    For the Ohm meter to work, do i need to connect the controller to a power source?

     

    so, ill need a power supply (transformer). This will connect to some sort of receiver.  The receiver that connects to the transformer and to the LED strip and the controller.  The controller will send a signal to the receiver to let the LED strips know what color and lights to use.

     

     

     

    the only receivers i see online are only for wireless connections, do you know of any wired receivers that could possibly take a 12 pin connection?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 6 years ago in reply to goatyhead

    No power needed - the resistance meter has its own power. It is not a good idea to measure resistance with power on the controller as it can overload the meter.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • dougw
    0 dougw over 6 years ago in reply to goatyhead

    No power needed - the resistance meter has its own power. It is not a good idea to measure resistance with power on the controller as it can overload the meter.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • goatyhead
    0 goatyhead over 6 years ago in reply to dougw

    thanks!!