Dev Tools
  • Products & Partners
  • More
Dev Tools
Forum Multiply two 16bit numbers, with a twist; post code
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 81 subscribers
  • Views 731 views
  • Users 0 members are here
  • 32bit
  • 8_bit
  • 32_bit
  • microchip
  • 16_bit
  • microprocessor
  • microcontrollers
  • programming
  • microcontroller
Related

Multiply two 16bit numbers, with a twist; post code

Catwell
Catwell over 16 years ago
I have a bit of an issue. I need to multiply two 16 bit numbers, (2 bytes each). But here is the difficulty, the uC registers are only 8 bits wide, (1 byte).  And the uC I am using has no multiply command, so I have to use the shift left & right, add process to get the multiplied result. And, the results may spill into 3 bytes.

Clock cycles are limited, so I need the tightest code possible. This is for a PIC 10F or 12F series.

If you have ever tried, accomplished it, let me know how you did it.

Or if you just need a challenge today, have a crack at it.
 
If you try, post the code here. Attach as a file, or just copy/paste.

Cabe
  • Sign in to reply
  • Cancel
  • akaka
    0 akaka over 16 years ago

    Dear Cabe

     

    I've found something I hope to be useful

     

    Chris

    Attachments:
    16_bit_example.txt.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • WestfW
    0 WestfW over 16 years ago

    Do you know about: http://www.piclist.com/techref/microchip/math/mul/index.htm ?

    Your choice: smal code (21 instructions) or fast execution.

    Also a bunch of "non-standard" multiply functions (12x12bit, etc)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Catwell
    0 Catwell over 15 years ago in reply to WestfW

    Thanks Chris and Bill,

     

    I did know about piclist. It is a mess of a site, and quite ugly to boot.

    However, those examples may give some insight.

     

    But, I really want to know base process behind the method, regardless of coding structure. Then I need to come up with the actual code for the processors in question. I want a deep understanding of how it is done before I copy some code.

     

    Cabe