Dev Tools
  • Products & Partners
  • More
Dev Tools
Forum Data Logger & Software combo needed
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 28 replies
  • Answers 2 answers
  • Subscribers 84 subscribers
  • Views 4232 views
  • Users 0 members are here
  • 8_bit
  • 32_bit
  • 16_bit
  • microcontrollers
  • embedded
  • development
  • microcontroller
Related

Data Logger & Software combo needed

Catwell
Catwell over 16 years ago

I am in the urgent need of a Data Logger / Data acquisition module with companion software. One stipulation, I need the software to be comfigurable without programming.


What have you used? What's good? I need any and all options.


Cabe

  • Sign in to reply
  • Cancel
Parents
  • Technocrat
    0 Technocrat over 16 years ago

    Hi Cabe,

     

    It might help if you were able to define your requirements a little more

    e.g.

    • Number of Channels
    • Readings per channel per second
    • Input type and range (volts, current etc)
    • Resolution (8,12,16bits etc)
    • Desired I/O interface (LAN, USB, RS232, GPIB)
    • Budget

     

    I liked Paul's suggestion of the 34970A.34970A., it's easy to use and has a very accurate 6.5 digit DMM as the measurement engine. It's also very flexible in terms of the cards you can add to the slots to create your solution, but it might be over kill, depending on what your doing. It also comes with some really nice intuitive software, Benchlink datalogger which needs no programming. You can also use Agilent VEE, which is a bit like Labview, to create a fully automated solution for an end user customer with a simple Start button which will then go off and run the tests, check pass fail and save the data. Admittedly this does take some programming, but it's graphical and pretty easy to use. I've also found Agilent to be really good in the past at sending me units for free for a week or two to play with and evaluate.

     

    Sticking with Agilent there's also their USB Range of products http://www.home.agilent.com/agilent/product.jspx?cc=GB&lc=eng&ckey=1486862&nid=-34321.0.00&id=1486862&pselect=SR.General. Which are really quite nice because you can use them individually or in a chassis if you need to scale your system up.

     

    There are a range of others of course, National Instruments are big in this area and then there are the lower cost PC based solution. The question is though, what exactly do you need?

     

    Ok I admit it I am a fan of Agilent equipment and shamelessly so!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Technocrat
    0 Technocrat over 16 years ago

    Hi Cabe,

     

    It might help if you were able to define your requirements a little more

    e.g.

    • Number of Channels
    • Readings per channel per second
    • Input type and range (volts, current etc)
    • Resolution (8,12,16bits etc)
    • Desired I/O interface (LAN, USB, RS232, GPIB)
    • Budget

     

    I liked Paul's suggestion of the 34970A.34970A., it's easy to use and has a very accurate 6.5 digit DMM as the measurement engine. It's also very flexible in terms of the cards you can add to the slots to create your solution, but it might be over kill, depending on what your doing. It also comes with some really nice intuitive software, Benchlink datalogger which needs no programming. You can also use Agilent VEE, which is a bit like Labview, to create a fully automated solution for an end user customer with a simple Start button which will then go off and run the tests, check pass fail and save the data. Admittedly this does take some programming, but it's graphical and pretty easy to use. I've also found Agilent to be really good in the past at sending me units for free for a week or two to play with and evaluate.

     

    Sticking with Agilent there's also their USB Range of products http://www.home.agilent.com/agilent/product.jspx?cc=GB&lc=eng&ckey=1486862&nid=-34321.0.00&id=1486862&pselect=SR.General. Which are really quite nice because you can use them individually or in a chassis if you need to scale your system up.

     

    There are a range of others of course, National Instruments are big in this area and then there are the lower cost PC based solution. The question is though, what exactly do you need?

     

    Ok I admit it I am a fan of Agilent equipment and shamelessly so!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Catwell
    0 Catwell over 16 years ago in reply to Technocrat

    Technocrat,

     

    I looked over the Agilent products, and they look like a definite option for me. The Benchlink datalogger software looks great too.

     

    All data logger programs, frontends, etc, always look like it was made in the Windows 3.11 days.

     

     

    Hardware selection is pretty flexible for me, I just need at least 12 bit sampling, and it has to interface via usb.

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Technocrat
    0 Technocrat over 16 years ago in reply to Catwell

    If you want USB connection you'll want to look at the  34972A34972A

     

    Looks like basically the same unit as the faithfull 34970A.34970A. but with USB Alternatively you could use the  82357B82357B USB to GPIB converter on a 34970A.34970A..

    Very handy the USB to GPIB converter, if ever you need to control HPIB / GPIB instruments with a modern computer, I seriously recommend investing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Catwell
    0 Catwell over 16 years ago in reply to Technocrat

    Technocrat,

     

    I forgot to mention the data logger must be small The  34972A34972A is a bit large and the lcd screens will never get used Any thoughts

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 16 years ago in reply to Catwell

    What about the Agilent  U2353AU2353A or one of the others from that range Neat little box USB no display I've got a  U2356AU2356A which is pretty good I bought it when I got fed up trying to get an NI board to work after 2 days of loading Gbyte drivers I still needed some other software horror I bought the Agilent thing and timed myself from opening the box to getting useful data on the PC about 20 minutes