Dev Tools
  • Products & Partners
  • More
Dev Tools
Forum Data Logger & Software combo needed
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 28 replies
  • Answers 2 answers
  • Subscribers 84 subscribers
  • Views 4221 views
  • Users 0 members are here
  • 8_bit
  • 32_bit
  • 16_bit
  • microcontrollers
  • embedded
  • development
  • microcontroller
Related

Data Logger & Software combo needed

Catwell
Catwell over 16 years ago

I am in the urgent need of a Data Logger / Data acquisition module with companion software. One stipulation, I need the software to be comfigurable without programming.


What have you used? What's good? I need any and all options.


Cabe

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 16 years ago

    Hi Cabe,

     

    Currently we are working in a datalogging system with RS232, ZigBee, 868Mhz or GRPS connectivity. The logging board has following features:

    - 2MByte of data storage.

    - Real time clock

    - 4 analog input channels for current sensing, temperature measurement, 0..20mV / 0..1V / 0..10V input voltages

    - RS232 usable as eiher communication device or as sensor input device

    - Dedicated sensor input for digital relative humidity and tempearture measurement

    - The logger board is designed to be batterypowered

    - The logger can be placed in a network with up to 1024 nodes

    - We also have gateways to LAN / WiFi

     

    Software uses a simple command set to

    - configure the sensors

    - control the measurement cycles

    - manage stored data

    - control network parameters of the device

     

    Currently we are also workin on an PC based application for data acquisition.

     

    Product will be available in the late summer this year. We are also interested in OEM clients (even for small amounts)

    We can do custom modifications to the sensor board. Feel free to contact us.

     

    Regards,

    Kris Demets

    Signum Engineering

    Belgium

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Catwell
    0 Catwell over 16 years ago in reply to e14 Contributor

    Kris,

     

    Can you post more information on your logger? What is the brand, where can I see it, etc?

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Catwell
    0 Catwell over 16 years ago in reply to e14 Contributor

    Kris,

     

    Can you post more information on your logger? What is the brand, where can I see it, etc?

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to Catwell

    Hi Cabe,

     

    The logger is still under development, which is our own brand. Where s-in the phase of beta-testing right now. Commercial documentation will ony be available as from september. So will be our website, where more information will be posted. The current version of our website www.signum-engineering.be is in dutch only and contains no information about the products currently under construction. (it's simply too soon for that).  The software protocol is also still under development, but is very much the same if you would like to connect over TCP/IP (through our Sensor-to-LAN interface), external RF device or the RS232.

     

    On server side, we are working on a database application to hold and visualize the captured data of  all sensors. This package will be on sale as well, probably by the end of the year

     

    The logger uses 4 channel of 16 bit analog to digital conversion, with a conversion rate of max. 400 Hz

    There is high precission current source output ranging from 10µA to 1mA

    A digital counter input can sense pulses up to 20kHz pulses

    The digital sensor interface is mainly designed to interface with our relative humidity and temperature sensor.

     

     

    The logger comes either as barebone PCB or as built-in in an IP67 housing (64x96x40mm) with an external 868 antenna. Target pricing for the barebone logger will be less than 200€ in small volumes.

     

     

     

     

    Kris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Catwell
    0 Catwell over 16 years ago in reply to e14 Contributor

    Kris,

     

    If you want, I could use your logger in my design. I could act as a test subject perhaps?

     

    What I have are 3 or more 4-20mA or 0-10V analog signal coming out of my monitoring hardware.

    I need the following:

    - At least 12 bit accuracy

    - To be able to display the data in real time on a laptop screen in real time

    - The ability to save the charts

    - A spreadsheet of the data

    - Possibly a way to directly print from the logging software

     

    Let me know if you can do all this.

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to Catwell

    Have you seen these folks: http://labjack.com/

     

    I have one of their U3-HV models and found it and its distributed software to be quite easy to work with. The PC side supports fairly arbitrary scripting and calculations on the raw input values to produce values for display and plotting. They also document their protocols and APIs with the stated goal of supporting use of their products in novel ways from third-party software.