Dev Tools
  • Products
  • More
Dev Tools
Forum What Propeller based projects have you worked on?
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 80 subscribers
  • Views 749 views
  • Users 0 members are here
  • microprocessor
  • microcontrollers
  • embedded
  • Design
  • development
  • microcontroller
  • propeller
Related

What Propeller based projects have you worked on?

Catwell
Catwell over 15 years ago

The Propeller microcontroller is one of the most inspiring chips I've ever read about. An 8-core, or 8-cog as they call it, MCU made by Parallax, that can be clocked from 32khz to 80Mhz. This chip was first introduced in 2006, it was ahead of the game. Only now has other MCU companies started down the multiple core path. It takes the MCU 4 clock cycles to execute a command, resulting in 20 MIPS (million instructions per second) per "cog," or 160 MIPS with all 8 cogs.

So much could be handled by this chip. In the QFN package, it would make an excellent multiple imput portable video game system processor. But I am getting ahead of myself. First I have to ask, what have you tried with a Propeller microcontrollerPropeller microcontroller?


Cabe

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 15 years ago +1
    Hi, when I first got in contact with this exciting piece of hardware, I also was wondering what would be possible with it. So, to get deeper into the structure, programming (especially the internal SPIN…
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    Hi,

     

    when I first got in contact with this exciting piece of hardware, I also was wondering what would be possible with it.

     

    So, to get deeper into the structure, programming (especially the internal SPIN-language) and the concept of parallel processing I selected a little project shown on the Parallax-Website: Thumper Internetradio... ( http://www.parallax.com/Thumper/tabid/848/Default.aspx ). And to be honest... I am still very impressed with how well it works... how easy it is to modify different parts... to get even more extensions running... how powerful it is.

     

    My first (and so far only) own project is a complete control for a webbased remote telescope (astronomy) and the according observatory. All is done by just this one controller... webserver and networking, motor control, analysis of different sensors (rain, temperature etc.), lighting control (dimming), heating and even a small basic-mp3-player for the beloved sound image There still is potential for further expansions... and a really great base of free libraries and codesamples available.

     

    Not thought about using it as a portable video game processor yet... the examples for this on the manufacturers website are kind of 80s style image

     

    Christian

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    I ordered the prototype board from Parallax of the propeller back in 2006...and have since ordered a number of development boards for various projects.  Unfortunately, most of those boards sit unused...I, like many others, am fascinated by the chip's design of independent, simultaneous 32 bit processors, each with its own small bit of memory.

     

    The problem I have found is implementing virtual devices on the propeller.  Unlike ARM or other micro-controllers, the Propeller is just a multi-processor silicon - no silicon based solutions for IO, timing, etc.  You need a UART?  One processor is now a UART.  Need a SPI controller?  One processor per SPI, please.  So, compared to a solution even as 'outdated' as, say, the NXP LPC2148FBD64,151LPC2148FBD64,151, which has 2 UARTs, 2 SPI, an I2C and USB (as well as 128kB of flash), the propeller comes up unfortunately short.

     

    What I envision the Propeller 'A' good for is an application where multiple inputs and direct port controls can be utilized - simple digital devices.  Now, eventually Parallax will come out with the Propeller 'B' and better (rumor has it that the next level of Propeller will increase the memory per cog to 16 or 32 kB and definitely double the IO).

     

    Keep an eye on Parallax - they are small, but dedicated (and located about 75 miles from me!).  The propeller has promise - but then, so did the Transputer, which died an untimely death when clock speeds went to GHz.