Dev Tools
  • Products
  • More
Dev Tools
Forum Parallel, redundant, Mosfets on DC motor control board
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 82 subscribers
  • Views 1288 views
  • Users 0 members are here
  • dc-dc
  • mosfet
  • controller
  • power_management
  • power_distribution
  • motion_control
  • power_supply
  • power_conversion
  • motor
Related

Parallel, redundant, Mosfets on DC motor control board

Catwell
Catwell over 15 years ago
imageimage
 
I was having a issue with some CNC machinery of mine, and I had to take apart the factory power systems in each. I noticed that the powering scheme has several paralleled mosfets. One of the mosfets, a D8020LD8020L, is more than enough for powering in the motor. But there were 5 in parallel. Is this a common practice for driving DC motors in machinery?
 
The above, blurry, pictures are from the machine's DC motor drive board.
 
Cabe
  • Sign in to reply
  • Cancel
Parents
  • jvdberg@ieee.org
    0 jvdberg@ieee.org over 15 years ago

    Hi Cabe,

    There must be a reason for using 5 devices in parallel.
    If the motor is not running, the impedance is very low and the start current might be very high.
    As a result of the inductance of the motor, the peak drain Voltage might be higher than the supply voltage.
    To operate the FET’s within the SOA (Safe Operating Area) the current per device must be derated.
    (See the SOA curve in the datasheet of the fet.)
    Another reason could be the dissipation in worst case conditions. The designer can use multiple standard fet and heatsink modules or heatsinks with different sizes. The larger size heatsinks cannot be mounted on a PCB because they are too heavy.
    Mosfets can easily be used in parallel because they have a positive temperature coefficient. The hottest device will draw the lowest current. This way the circuit will stabilize itself.
    Bipolar transistors  have a negative temperature coefficient, causing the hottest device to draw the highest current.
    This could lead to thermal runaway and failure of the device with the lowest resistance.
    When transistors are used in parallel, resistors are necessary for equal distribution of the current over the devices.
    A disadvantage of using multiple fets in parallel is the larger drain – gate capacity, that requires a higher drive current. Replacing a single fet by multiple fets in parallel might lead to instability and oscillations unless a separate drive circuit is used for each fet.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jvdberg@ieee.org
    0 jvdberg@ieee.org over 15 years ago

    Hi Cabe,

    There must be a reason for using 5 devices in parallel.
    If the motor is not running, the impedance is very low and the start current might be very high.
    As a result of the inductance of the motor, the peak drain Voltage might be higher than the supply voltage.
    To operate the FET’s within the SOA (Safe Operating Area) the current per device must be derated.
    (See the SOA curve in the datasheet of the fet.)
    Another reason could be the dissipation in worst case conditions. The designer can use multiple standard fet and heatsink modules or heatsinks with different sizes. The larger size heatsinks cannot be mounted on a PCB because they are too heavy.
    Mosfets can easily be used in parallel because they have a positive temperature coefficient. The hottest device will draw the lowest current. This way the circuit will stabilize itself.
    Bipolar transistors  have a negative temperature coefficient, causing the hottest device to draw the highest current.
    This could lead to thermal runaway and failure of the device with the lowest resistance.
    When transistors are used in parallel, resistors are necessary for equal distribution of the current over the devices.
    A disadvantage of using multiple fets in parallel is the larger drain – gate capacity, that requires a higher drive current. Replacing a single fet by multiple fets in parallel might lead to instability and oscillations unless a separate drive circuit is used for each fet.