Dev Tools
  • Products
  • More
Dev Tools
Forum Parallel, redundant, Mosfets on DC motor control board
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 82 subscribers
  • Views 1288 views
  • Users 0 members are here
  • dc-dc
  • mosfet
  • controller
  • power_management
  • power_distribution
  • motion_control
  • power_supply
  • power_conversion
  • motor
Related

Parallel, redundant, Mosfets on DC motor control board

Catwell
Catwell over 15 years ago
imageimage
 
I was having a issue with some CNC machinery of mine, and I had to take apart the factory power systems in each. I noticed that the powering scheme has several paralleled mosfets. One of the mosfets, a D8020LD8020L, is more than enough for powering in the motor. But there were 5 in parallel. Is this a common practice for driving DC motors in machinery?
 
The above, blurry, pictures are from the machine's DC motor drive board.
 
Cabe
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    Hello,

     

    one important differentiation we need to make here is whether it is a linear or switch-mode drive. Today, and especially in this power range, pretty much all drive circuits are switch-mode. The motors being used are brushless DC motors in many cases, for which a "frequency inverter" is needed. The minimum number of phases for an electrical motor to effectively determine rotational direction is 3, so you should be seeing three half bridges, or 6 sets of switches in the inverter.

    For lower-voltage motors (think forklifts), the currents are very high for the same power, as the voltage is lower. So you'll need more current-handling capability in the switches. Moreover, the worst case condition for the current is determined by the mechanical parts the motor is driving, e.g. when it is blocking, or at startup. Third, the time until any overcurrent protectio ncircuit can react needs to be considered as well. These factors lead us to rather large design margins that need to be implemented, hence the paralleling of so many MOSFETs. In fact, in forklifts it is not uncommon to see 30-40 MOSFETs in parallel.

    Key to successful paralleling in linear applications are given in the previous posts. For switching applications, some of this applies as well. The most important factor here is a "good enough" match of the threshold voltage of the MOSFETs. Imagine at turn on: The MOSFET with the lowest threshold voltage will turn on first, and as the gate voltage continues to rise the other MOSFETs will follow. However, that first MOSFET will see high currents, potentially leading to destruction.

    On the temperature coefficient, yes MOSFETs have a positive tempco if operated above a certain current level (which is almost always the case in switching power applications). If you look at the diagram of drain current versus gate voltage for different temperatures, you will see all these lines cross in one point, where the temperature coefficient is literally zero.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    Hello,

     

    one important differentiation we need to make here is whether it is a linear or switch-mode drive. Today, and especially in this power range, pretty much all drive circuits are switch-mode. The motors being used are brushless DC motors in many cases, for which a "frequency inverter" is needed. The minimum number of phases for an electrical motor to effectively determine rotational direction is 3, so you should be seeing three half bridges, or 6 sets of switches in the inverter.

    For lower-voltage motors (think forklifts), the currents are very high for the same power, as the voltage is lower. So you'll need more current-handling capability in the switches. Moreover, the worst case condition for the current is determined by the mechanical parts the motor is driving, e.g. when it is blocking, or at startup. Third, the time until any overcurrent protectio ncircuit can react needs to be considered as well. These factors lead us to rather large design margins that need to be implemented, hence the paralleling of so many MOSFETs. In fact, in forklifts it is not uncommon to see 30-40 MOSFETs in parallel.

    Key to successful paralleling in linear applications are given in the previous posts. For switching applications, some of this applies as well. The most important factor here is a "good enough" match of the threshold voltage of the MOSFETs. Imagine at turn on: The MOSFET with the lowest threshold voltage will turn on first, and as the gate voltage continues to rise the other MOSFETs will follow. However, that first MOSFET will see high currents, potentially leading to destruction.

    On the temperature coefficient, yes MOSFETs have a positive tempco if operated above a certain current level (which is almost always the case in switching power applications). If you look at the diagram of drain current versus gate voltage for different temperatures, you will see all these lines cross in one point, where the temperature coefficient is literally zero.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer