Dev Tools
  • Products
  • More
Dev Tools
Forum Measuring pressure in an air duct
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 82 subscribers
  • Views 777 views
  • Users 0 members are here
  • test
  • dev_kits
  • measure
  • knode
  • Design
  • flow
  • sensor
Related

Measuring pressure in an air duct

ZeroSizeObject
ZeroSizeObject over 15 years ago

I have an odd problem to overcome. I need to measure pressure changes in air ducts, from small 2" to much larger.

 

Pressure changes come every time the air systems are turned on, but more importantly when something is blocking airflow.

 

 

I was thinking about placing turbine like fans in the ducts and measure the speed changed in the fans themselves. But, I am not sure if this is the most accurate option.

 

Any thoughts?

 

Zero

  • Sign in to reply
  • Cancel
  • DAB
    0 DAB over 15 years ago

    Hi Zero,

     

    Do you need to measure the actual air pressure or just if air is moving through the vent?  There are several easy ways to just verify air flow, but I not aware of any easy way to measure the true air pressure without putting in a lot of pressure sensors.

    If all you need is air movement, you can install small magnets on strips of a thin film and then use a reed switch or inductive coil to indicate if the air is moving.

     

    Hopefully this helps you better quantify your problem.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Catwell
    0 Catwell over 15 years ago in reply to DAB

    Zero,

     

    Back pressure in the system would, indeed, cause the vent fan to slow down. Measure changes in the motor itself. Take samples of the motor profiles and then check to see if the motor is still within range. When something does block airflow, the motor should show a dramatic change.

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    I think that most reliable solution would be using mass air flow sensors like those used in cars (they should be widely available). Check this pdf: http://www.autoshop101.com/forms/h34.pdf it gives an view to overall principle of operation.