Dev Tools
  • Products & Partners
  • More
Dev Tools
Forum Why would I ever use Matlab?
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 80 subscribers
  • Views 1103 views
  • Users 0 members are here
  • 8_bit
  • 32_bit
  • 16_bit
  • programming
  • matlab
  • microcontroller
Related

Why would I ever use Matlab?

Dig
Dig over 15 years ago

Besides having to take a class in Matlab in college, back almost 10 years now. I have never used it for anything. Recently, I have been seeing Matlab being a requirement for new jobs. Is it a language I should learn? What is the benefit of it? And can code be easily dropped on micro-controllers?

 

Dig

  • Sign in to reply
  • Cancel
Parents
  • Jorge_Garcia
    0 Jorge_Garcia over 15 years ago

    Hi Dig,

     

    MATLAB is the industry standard computing platform. It's used for high powered scientific computing and algorithm testing. You would only use it if you were developing sophisticated models of engineering phenomena or needed to perform any sophisticated mathematical analysis.

     

    Many would claim that it's biggest benefit is that it is a mature program that is heavily supported and allows for quick protoyping of design ideas. For example lets say you're designing a control system, using MATLAB you can quickly create a plant model and start experimenting with a controller such as a PID system. Without ever building the system, you can have MATLAB obtain the ideal control parameters subject to some set of constraints. You could then see bode plots and such all within the same environment.

     

    MATLAB is much more than this, but I think this gives some point of reference. The very major downside of MATLAB is the price tag, it is very expensive software well outside the reach of most individuals(depending on the configuration can cost $10,000+). This has lead many to seek out alternatives and there are a few good open source solutions. Octave is command line based but the syntax is very similar to Matlab and over all it works fairly well. I personally use the Numpy+Scipy+Matplotlib Python libraries to get some of the functionality available built-in to Matlab. The open source alternatives are no where near as developed as MATLAB, but they can be had for the low price of FREE and I can make payments on FREE.

     

    From what I've described I'm sure you have realized that MATLAB is not a seperate language persay but rather a very powerful computing tool with it own proprietary programming language. It's not really meant to create code for microcontrollers, however one of the available modules for it allow you to create C code from the MATLAB code your controller or whatever is based on. You should then be able to clean up the code a little and drop it into a micro. I've never used the feature so I can't say anything about how  well it works.

     

    I hope this helps clear up some confusion.

     

    Best Regards,

    Jorge Garcia

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 15 years ago in reply to Jorge_Garcia

    Interesting you should ask ?

     

    I've had MATLAB for many years and I'm just wondering if I should renew my subscription (£1113 this year for a small subset of the total toolset) yet again. I do use it quite often for data analysis (it will easily handle large data sets that choke Excel) but rarely for modelling.

    I could do the data analysis with other tools but the MATLAB suite is pretty good for system modelling (but getting VERY expensive).

    You can also look at Freemat (tiny subset of all that Mathworks offer but free !)

    The Mathworks seems to be moving in a slightly different direction from me so that I find very little difference using release 2007 or 2010 (but I paid £3000 to get from one to the other !).

    So I hope this rambling helps you a bit (it's helped me focus my ideas !).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 15 years ago in reply to Jorge_Garcia

    Interesting you should ask ?

     

    I've had MATLAB for many years and I'm just wondering if I should renew my subscription (£1113 this year for a small subset of the total toolset) yet again. I do use it quite often for data analysis (it will easily handle large data sets that choke Excel) but rarely for modelling.

    I could do the data analysis with other tools but the MATLAB suite is pretty good for system modelling (but getting VERY expensive).

    You can also look at Freemat (tiny subset of all that Mathworks offer but free !)

    The Mathworks seems to be moving in a slightly different direction from me so that I find very little difference using release 2007 or 2010 (but I paid £3000 to get from one to the other !).

    So I hope this rambling helps you a bit (it's helped me focus my ideas !).