Dev Tools
  • Products
  • More
Dev Tools
Forum PIC 16F877 w/ GSM Modem, need help w/ design
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 81 subscribers
  • Views 479 views
  • Users 0 members are here
  • controller
  • modem
  • gsm
  • power_supply
  • microcontroller
  • pic
Related

PIC 16F877 w/ GSM Modem, need help w/ design

Dig
Dig over 14 years ago
I want to interface a PIC 18F877 with a GSM Modem. Can I interface with the modem through a terminal program? Anyone ever interfaced a modem like this with any type of micro-controller?
Dig
  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Hi Dig

     

    I can recommend the use of my development kits. Please go to http://www.emkernel.com/

    You can consider getting the

     

    EasyPIC6

    http://www.emkernel.com/collections/development-tools/products/pic-development-tools

     

    or the Ready-for-PIC

    http://www.emkernel.com/collections/development-tools/products/ready-for-pic

     

    We also supply GSM modems that provide seamless integration with these boards.

    The compiler library provides readily available APIs that can communicate with the

    GSM boards. This speeds up the learning curve and gives you more time to focus on

    other aspects of the project.

     

    Please feel free to contact me at ravi.suppiah@emkernel.com to find out more!

     

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Kelv
    0 Kelv over 14 years ago

    Hi Dig,

    Is there a reason you are looking at using the 16f877? The most common interface for GSM modules is a usart and from memory I'm pretty sure that the 16f877 only has one hardware USART, whilst not show stopping it means that you will need to bit bang either the modem interface or the PC interface and means you have less resources available for anything else you are needing to impliment. You might want to consider using a later Pic variant with 2 uarts or even USB.

     

    Have you got a GSM module in mind?

    Again the ones I am familiar with use either a variant of the Hayes command set, which it really easy to use, or a proprietry data protocol. Still not too difficult to use but will require more time pouring over datasheets. So yes, in some cases you can talk directly to the modem but it is very hardware dependant. Oh and dont forget the Pic is a 5v device and a lot of the newer GSM modules are 3.3v only so you need voltage translation, its a terrible thing to watch the smoke escaping image

     

    If you want to provide more info on the project I would be happy to discuss it with you further, or drop an email to techsales@farnell.com and mark it for my attention.