Dev Tools
  • Products
  • More
Dev Tools
Forum Op amp circuit not amplifying properly, help
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 82 subscribers
  • Views 1005 views
  • Users 0 members are here
  • gain
  • knode
  • Design
  • amplify
  • tools
  • filter
  • op_amp
Related

Op amp circuit not amplifying properly, help

Latch
Latch over 14 years ago
I have an issue.
I want to amplify a signal through 2 op amps. The feedback resistor is between the image pin and the output. (pin 2 and 6 of the 741op amp). The resistor ration (r2/r1) is 150. However, I only get an amplification of 5x. Different resistors for r2 yields the same result. I even changed the op amp, same issue.

The second op amp in the series works fine, but stage one refuses to function. The cap I am using is at 0.47uf and the feedback resistor is 1.5M.

What is the problem?
 

image
 
Above: This is what the circuit is based on.
 

Latch
  • Sign in to reply
  • Cancel
Parents
  • jvdberg@ieee.org
    0 jvdberg@ieee.org over 14 years ago

    The internal resistance of the transducer must be added to the 10k resistor at the input of the first opamp. If the internal resistance of the transducer is 200 k-ohm, the gain is 5 * A solution for the low gain could be connecting the transducer to the non inverting input of the opamp.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Latch
    0 Latch over 14 years ago in reply to jvdberg@ieee.org

    I did not think of that, thank you. I will see if that helps...

     

    Latch

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • RWM
    0 RWM over 14 years ago in reply to Latch

    You can find information about designing ampifiers for piezoelectric ultrasonic transducers there:

    http://130.89.85.15/electronics/ultrasound/Low%20output%20noise%20amp%20for%20piezo%20trancdurs.pdf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • RWM
    0 RWM over 14 years ago in reply to Latch

    You can find information about designing ampifiers for piezoelectric ultrasonic transducers there:

    http://130.89.85.15/electronics/ultrasound/Low%20output%20noise%20amp%20for%20piezo%20trancdurs.pdf