Dev Tools
  • Products & Partners
  • More
Dev Tools
Forum ESD protection and GND plane issues for automotive circuit
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 79 subscribers
  • Views 448 views
  • Users 0 members are here
  • mosfet
  • transistor
  • knode
  • Design
  • automotive
  • gnd
  • esd
Related

ESD protection and GND plane issues for automotive circuit

Latch
Latch over 15 years ago
I am making a datalogger circuit for automobiles. I am at an impasse. What is more important in automotive design, and smooth GND plane or ESD protection on each input?
 
I have cleared some space on the PCB, only on the bottom layer unfortunately. If I add ESD protection is limits the amount of the GND by almost half.
 
Latch
  • Sign in to reply
  • Cancel
Parents
  • Catwell
    0 Catwell over 15 years ago
    When it comes to automotive, many of the parts are made by someone else. So, keep in mind that no one is protecting their part, or also making sure their part does not interfere with others.
     
    Some rules for design:
    Place all the ESD components (including caps) as close to the connector as possible.
     
    The ground plane often gets segmented up. Ground return current is the most overlooked current. Always allow the ground current to follow the same path as the supply current.
     
    Digital should be separate from analog. Does your design have an IC with both digital and analog?
     
    Keep the ground plane as solid as possible. If the ground starts bouncing, sits at a higher or lower potential, you are stealing voltage from your system. Big trouble. If the IC is supposed to run at 5V, would you want it at 4.75V?
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Catwell
    0 Catwell over 15 years ago
    When it comes to automotive, many of the parts are made by someone else. So, keep in mind that no one is protecting their part, or also making sure their part does not interfere with others.
     
    Some rules for design:
    Place all the ESD components (including caps) as close to the connector as possible.
     
    The ground plane often gets segmented up. Ground return current is the most overlooked current. Always allow the ground current to follow the same path as the supply current.
     
    Digital should be separate from analog. Does your design have an IC with both digital and analog?
     
    Keep the ground plane as solid as possible. If the ground starts bouncing, sits at a higher or lower potential, you are stealing voltage from your system. Big trouble. If the IC is supposed to run at 5V, would you want it at 4.75V?