Dev Tools
  • Products
  • More
Dev Tools
Forum Help designing a solution for this problem!
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 10 replies
  • Subscribers 83 subscribers
  • Views 1928 views
  • Users 0 members are here
Related

Help designing a solution for this problem!

e14 Contributor
e14 Contributor over 14 years ago

Hi folks!

 

I am wanting to develop a chip which will do the following:

 

Take Keyboard input via USB, record something about the input - and then pass the input onto the computer. I want the recording of 'something' saved on an sdcard or some form of memory so it is persistent across runs.

 

So - i started with one of these: http://uk.farnell.com/ftdi/v2dip2-32/module-dev-32-pin-2x-usb-vnc2/dp/1825832 However I have found the chip difficult to code - being entirly c based - and do not like the platform in general, has so many bugs and no community around to support it.

 

The chip was suitable because it had 2 USB ports, meaning I could plug the keyboard into one of them, then a male to male cable in the other to connect it back to the computer. I then bought an sd card reader chip for saving state and a FT232 UART to help me debug. Problem was VOS which is the OS layer the VNC2 runs was just massively flawed and caused so many problems debugging etc

 

I am a massive Java fan - and was wondering perhaps if there is a chip out there which supports Java? Would the above be possible via a chip which runs Java? I am looking for any suggestions!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    No replies yet!? I was recommended this community for aid and not received any so far after nearly 20 hours! Is there something I have missed out - or have I asked this in the wrong section?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    No replies yet!? I was recommended this community for aid and not received any so far after nearly 20 hours! Is there something I have missed out - or have I asked this in the wrong section?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • DAB
    0 DAB over 14 years ago in reply to e14 Contributor

    Hi Andy,

     

    The Parallax Propeller chip runs SPIN, which is a Java like language.  It would give you all the power you would need to build your circuit with.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to DAB

    Hmm I really would prefer to be able to use a full Java stack...