Dev Tools
  • Products
  • More
Dev Tools
Forum Bluetooth Low Energy Expansion Board based on BlueNRG for STM32
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 80 subscribers
  • Views 457 views
  • Users 0 members are here
  • bluetooth
  • x-nucleo-idb04a1
  • stm32
  • bluenrg
  • nucleo
Related

Bluetooth Low Energy Expansion Board based on BlueNRG for STM32

e14 Contributor
e14 Contributor over 11 years ago

Es-ce que la carte X-NUCLEO-IDB04A1 est compatible pour fonctionner directement sur une carte Arduino UNO, j'entend au niveau de la compatibilité 3V3 - 5V ?

 

Merci

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi Arnauld,

     

    The X-NUCLEO-IDB04A1  EXPANSION BOARD is compatible with the Arduino uno R3 connector physical layout as far as pin placement.  However, the Bluetooth IC on the board is not 3.3V tolerant, and there is no level translator on the board.  Therefore, I would not recommend to use it directly on a Arduino board with 5V IO.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi Arnauld,

     

    The X-NUCLEO-IDB04A1  EXPANSION BOARD is compatible with the Arduino uno R3 connector physical layout as far as pin placement.  However, the Bluetooth IC on the board is not 3.3V tolerant, and there is no level translator on the board.  Therefore, I would not recommend to use it directly on a Arduino board with 5V IO.