Dev Tools
  • Products
  • More
Dev Tools
Forum Beaglebone PRU Debugging
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 79 subscribers
  • Views 398 views
  • Users 0 members are here
  • Bob
  • beaglebone-black
  • bbb-pru
Related

Beaglebone PRU Debugging

e14 Contributor
e14 Contributor over 11 years ago

I've been working through Derek Molloys book, http://exploringbeaglebone.com/, for a student project. It's been an excellent resource, but I've finally hit a snag.

For anyone else fusing the book, I'm in Chapter 13, in the section on Utilizing Regular Linux GPIOs.

 

I've deviated from the examples he provides by using PRU1 instead of PRU0. I've successfully used the PRUs to flash LEDs through the enhanced IO pins that tie directly to the PRU. Now I am trying to flash LEDs using the GPIO, and I'm not succeeding. I am hoping that someone here will take a look at my code and be able to spot something I've missed. I've thoroughly tested the circuit, and I am certain the the off-board electronics are working correctly. I'm confident that its either something I've missed on the dtbo or in the assembler code. But (I think) I've carefully checked my code against the examples, and I cannot spot my error.


After loading the dtbo, all the relevant GPIO pins are in mode 0x07.


I've set one enhanced IO pin to light as well, and it blinks when it is supposed to, so I know the program is running with the correct timing. None of the GPIO fins will flash, however.


 

// PRUSS program to trigger 10 output pins in sequence for a calculated time

// then waits for input pins to go high and starts counter

// Written by Alwyn Smith for Firefighting Drone Challenge

 

 

.setcallreg   r29.w0    // set a register for CALL/RET

.origin 0               // offset of start of program in PRU memory

.entrypoint SETUP      // program entry point used by the debugger

 

 

#define PRU0_R31_VEC_VALID  32;

#define PRU_EVTOUT_0        3

#define PRU_EVTOUT_1        4

#define DELAY               100000000 //#instructions for .5 second

#define GPIO0   0x44e07000  //GPIO Bank 0, see AM335x TRM tab 2.2 Peripheral Map

#define GPIO1   0x4804c000  //GPIO Bank 1

#define GPIO2   0x481ac000  //GPIO Bank 2

#define GPIO3   0x481ae000  //GPIO Bank 3

#define GPIO_CLEARDATAOUT   0x190  //for clearing GPIO registers

#define GPIO_SETDATAOUT     0x194  //for setting GPIO registers

#define GPIO_DATAOUT        0x138  //for reading GPIO registers

 

 

#define GPIO0_8     1<<8   //P8_35 gpio0[8]     Output - bit 8

#define GPIO0_9     1<<9   //P8_33 gpio0[9]     Output - bit 9

#define GPIO0_10    1<<10  //P8_31 gpio0[10]    Output - bit 10

#define GPIO0_11    1<<11  //P8_32 gpio0[11]    Output - bit 11

#define GPIO2_14    1<<14  //P8_37 gpio2[14]    Output - bit 14

#define GPIO2_15    1<<15  //P8_38 gpio2[15]    Output - bit 15

#define GPIO2_16    1<<16  //P8_36 gpio2[16]    Output - bit 16

#define GPIO2_17    1<<17  //P8_34 gpio2[17]    Output - bit 17

#define GPIO2_25    1<<25  //P8_30 gpio2[25]    Output - bit 25

 

 

SETUP:

   LBCO   r0, c4, 4, 4    //load SYSCFG register to r0 (use c4 const address)

   CLR    r0, r0, 4       //clear bit 4 (STANDBY_INIT)

   SBCO   r0, c4, 4, 4    //store the modified r0 back at the the load addr

   LDI    r7, 30          //set the number of blink cycles

 

START:

   MOV r8, DELAY    //reset clock counter

 

TRIGGER:

   //set each output pin high to start trigger pulse

   SET    r30.t8        //set P8_27 high

   CALL   DELAYON

 

TRIGGER_P8_30:

    MOV     r1, GPIO0 | GPIO_SETDATAOUT  //load address for GPIO Set Data to r1

    MOV     r2, GPIO0_8            //write GPIO_8 to r2

    SBBO    r2, r1, 0, 4           //write r2 to the r1 address -LED ON

    MOV     r8, DELAY    //reset clock counter

    CALL    DELAYON

 

TRIGGER_P8_31:

    MOV     r1, GPIO0 | GPIO_SETDATAOUT  //load address for GPIO Set Data to r1

    MOV     r2, GPIO0_9            //write GPIO_9 to r2

    SBBO    r2, r1, 0, 4           //write r2 to the r1 address -LED ON

    MOV     r8, DELAY    //reset clock counter

    CALL    DELAYON

 

   //set each output pin low to finish trigger pulse

    CLR   r30.t8         //set P8_27 low

 

KILL_P8_30:

    MOV     r1, GPIO0 | GPIO_CLEARDATAOUT  //load address for GPIO Clear Data to r1

    MOV     r2, GPIO0_8            //write GPIO_8 to r2

    SBBO    r2, r1, 0, 4           //write r2 to the r1 address -LED OFF

    MOV     r8, DELAY    //reset clock counter

    CALL    DELAYON

 

KILL_P8_31:

    MOV     r1, GPIO0 | GPIO_CLEARDATAOUT  //load address for GPIO Clear Data to r1

    MOV     r2, GPIO0_9            //write GPIO_9 to r2

    SBBO    r2, r1, 0, 4           //write r2 to the r1 address -LED OFF

    MOV     r8, DELAY    //reset clock counter

    CALL    DELAYON

 

CHECK:                          //check to see if loop should continue

    SUB   r7, r7, 1              //reduce the cycle count by 1

    QBNE  START, r7, 0           //if cycle count != 0, then start new cycle

    QBEQ  END, r7, 0             //if r1 == 0, then end the program

 

 

DELAYON:                        //start a 1 second counter

    SUB    r8, r8, 1             //decrement the counter by 1

    QBNE   DELAYON, r8 , 0       //while count !=0, continue counting

    RET                          //return to calling procedure

 

 

END:

    MOV R31.b0, PRU0_R31_VEC_VALID | PRU_EVTOUT_0

    HALT