Dev Tools
  • Products
  • More
Dev Tools
Forum L298 current sensor pin, convert pulsed current signal to consumption flag
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 20 replies
  • Answers 2 answers
  • Subscribers 84 subscribers
  • Views 5470 views
  • Users 0 members are here
Related

L298 current sensor pin, convert pulsed current signal to consumption flag

modelrailwaycat
modelrailwaycat over 11 years ago

Hello,

 

I am designing a small, simple 12V motor controller fed by a L298 H-bridge driver. The H-bridge input pins are supplied by means of PWM at 40 Hz. The motor can be connected or disconnected from the output even with the input and enable on. For this reason, I am interested in adding additional circuitry in order to obtain a binary signal of consumption using the current sensor pins; that is obtain a permanent high level while some current is detected and a permanent low level when no current is detected (after at least 1 period, but this is flexible).

 

The idea is to use a 0.5 ohm resistor to connect the sense pin to ground, and then use the voltage across the resistor to obtain the signal. I consider that the voltage measured will be from 5 mV to 1V and the Duty Cycle can be down to 1%. Because the sensor signal is also pulsed, I need somehow to filter it and obtain an stable output while consumption is 'on'. The problem is that I had not success to set properly a low-pass filter plus op-amp buffer configuration from this signal working reliably with all the mentioned conditions. I also tried to pre-amplify the sensor signal with another op-amp, then output that into the low-pass filter plus buffer, but had no success too.

 

Any idea is appreciated. Thank you very much!

  • Sign in to reply
  • Cancel

Top Replies

  • D_Hersey
    D_Hersey over 11 years ago +2 suggested
    Can you draw it up? What op-amp are you using? Not all op amps have common mode input range all of the way to BoS.
  • D_Hersey
    D_Hersey over 11 years ago +2
    "If you are going to reverse the current, you will need to set up a different reference voltage as with everything referred to 0V you will not get a negative swing. And your comparator will have to work…
  • peterjcs23
    peterjcs23 over 11 years ago in reply to modelrailwaycat +1
    Hi John, is your motor turning ok? If you put a DVM across Rsense what voltage do you see when turning and when stationary? Do you have a scope to look at waveforms? Peter
Parents
  • D_Hersey
    0 D_Hersey over 11 years ago

    If you have a spare -5V supply you could try something along these lines, this might be faster but a little less accurate.  I think Peter had the idea awhile ago, IIRC.

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 11 years ago

    If you have a spare -5V supply you could try something along these lines, this might be faster but a little less accurate.  I think Peter had the idea awhile ago, IIRC.