Dev Tools
  • Products
  • More
Dev Tools
Forum Data transfer in PSoc 4
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 81 subscribers
  • Views 667 views
  • Users 0 members are here
  • usb
Related

Data transfer in PSoc 4

e14 Contributor
e14 Contributor over 11 years ago

Hi everyone,

Nik here. I am doing a project on PSoC 4 pioneer kit. The project is to replace a Berthold 2040 Amplifier/ Counter with additional 8 bit CPU and RS232 read out.

 

In my project, two inputs are established, one digital and the other analog with amplifier and comparator of PSoC. Pulses on either of the inputs are counted for a preselected time. LCD & Buttons shall be realised by a proper arduino shield. Start, Stop and Reset of the counter and the preselection of measurement time are selected by a menu which is displayed on the LCD.

 

I am done with half of my project and now I need your assistance in doing the data transfer between PSoC and PC.

 

ie, Every second, the counter content ( pulse/ second)  is send to a PC via USB.

ie, The transfer of three values ( measure 1, measure 2, time ).

 

In further detail, About two times a second, the counter content is displayed on a LCD on line 1. Time selected and remaining seconds of measurement on line 2 of LCD.

 

I need to get the LCD content displayed on my PC screen.

 

Should I be using UART, I2C or SPI for the same along with a hyperterminal or putty ?

Any help is appreciated.

 

Thanks & Regards,
Nikhil Kurian.

 

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 11 years ago +1
    The PSOC4 Pioneer Kit it has a USB interface via a UART. The connection looks like a UART to the PSOC4 and the drivers for the UARTs are already in PSOC Creator. Here is an example with the Pioneer Kit…
  • clem57
    0 clem57 over 11 years ago

    ie, Every second, the counter content ( pulse/ second)  is send to a PC via USB.

    ie, The transfer of three values ( measure 1, measure 2, time ).

    Does that go to PC to be displayed? Yes, then send LCD along with it.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to clem57

    Yes clem. I have done it till thé counter content being displayed on the lcd. Now I need to transfer thé same data to thé pc and want it to be displayed there as well.

     

    Any assistance is appreciated.

    Thanks,

    Nik

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 11 years ago

    The PSOC4 Pioneer Kit it has a USB interface via a UART.

    The connection looks like a UART to the PSOC4 and the drivers for the UARTs are already in PSOC Creator.

    Here is an example with the Pioneer Kit:

    PSoC 4 Pioneer Kit Community Project#04 - USB-UART Utility

    Any terminal emulator program on the PC will display serial data from the Pioneer Kit.