Dev Tools
  • Products
  • More
Dev Tools
Forum Latching Start Circuit using Flip Flops
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 16 replies
  • Subscribers 82 subscribers
  • Views 3196 views
  • Users 0 members are here
  • logic
  • digital
  • flip_flops
Related

Latching Start Circuit using Flip Flops

oldmanraskers
oldmanraskers over 11 years ago

I have been working on a CPLD project to run a state machine that will control a bunch of solenoids - I have mostly finished the hardware but now I'm moving onto the state machine. I can make the state machine conintually run, but what I really want is to implement a latching start/stop circuit that uses momentary pushbuttons... I want to be able to press start and have the state machine run (but I don't want to have to keep the start button pressed). I then want to press the stop button and make the state machine pause (again, i don't want to keep the stop button pressed). And finally, if I start the state machine but don't press the stop button, then I want the state machine to run to the last state and automatically stop. Thinking to years gone by, I kind of remember something about making a k-map for the start and stop inputs and building some s-r flip flop truth tables, but I can't remember and I also can't find exactly what I need on the web. I would be very grateful is someone could give me pointers on the method - I know I'm almost there image but it's years since I was taught this stuff and I simply can't remember image

Regards, MR.

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 11 years ago in reply to michaelkellett +1
    Did I miss something? Where is the logic for the state machine? Does it use a clock? Clem Edited: Ok see it now as attached.
  • michaelkellett
    michaelkellett over 11 years ago in reply to johnbeetem +1
    Hi John, I don't think we'll ever agree on this so I'm not trying to convert you When I design FSMs for FPGAs, I always do the state assignment (i.e., state encoding) by hand because I have no confidence…
Parents
  • johnbeetem
    0 johnbeetem over 11 years ago

    MR -- you might get something useful from my 'blog "First Experiments with the ValentF(x) LOGI-Pi", specifically section "Experiment 2".  That section has a design for a 4-bit binary counter with reset and hold, written in Verilog.

     

    As clem57 says, for CPLDs and FPGAs you probably want a clocked state machine with an oscillator providing a clock.  Usually oscillators are really fast, so you'll need to divide down to something reasonable.  My example has a 50 MHz oscillator, since that's what comes with the LOGI-Pi.  But you can make something a lot slower, perhaps with an LMC555 timer.

     

    The actual counter update is very simple in Verilog:

     

    always @(posedge Mclk or posedge reset)

    if (reset) K <= 0; else if (clk4Hz) K <= K+up;

     

    This says if the 50MHz master clock Mclk has a positive edge (rises) or the asynchronous reset has a positive edge, execute the if statement.  If reset is high, clear the counter state K to 0, otherwise if clk4Hz is high (it pulses for one cycle every 1/4 second) update K to K+up where up is the counter enable (connected to a push button).  The + operator is addition: logical OR is the | or || operator from C.  If reset=0 and clk4Hz=0 leave K as it is.

     

    The vendor's synthesizer does the logic minimization so you don't ever see K-maps or excitation tables and all that great theory from your undergrad days.

     

    You do need to be concerned about switch bounce.  I ignored it in my example because K only updates at 4 Hz and the chances of updating K exactly when you press or release a button is so slight that you probably won't see it in practice.  In a serious circuit that controls something real like solenoids you do need to be concerned.

     

    Hope this helps!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • oldmanraskers
    0 oldmanraskers over 11 years ago in reply to johnbeetem

    The CPLD is clocked at 10MHz using a VCO which I need because I plan to run a timer and so forth... but I don't really want the state machine to be paused by removing the clock source, instead I want to control it via start and stop buttons, in addition to having it automatically stop when it reaches its last state. I'm not sure what Clem means when he says a full logic reset is needed to restart - that sounds like something I want to avoid because I want to pause then continue, not pause then restart... or maybe I'm misunderstanding image  but I will take a look at the reference you made, John.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to oldmanraskers

    Here's some VHDL which might give you some ideas. Life's too short to simulate this in the Quartus horror (when you've got something better which I have) so you'll need to bite that bullet yourself. It seems to mainly work (ie all the bits I tested worked !).

    It uses 39% of the logic in your 160 ff CPLD so you may be needing to use a bigger one.

     

    Get back to me about the bits that don't make sense.

     

    All comments and criticisms of my VHDL style welcome (from whatever source). Please note (in said style) the single process not obviously Mealy or Moore state machine -works for me and Synplfy gets it.

     

    MK

    Attachments:
    lock.vhd.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • oldmanraskers
    0 oldmanraskers over 11 years ago in reply to michaelkellett

    Thanks for taking the time do dot his Michael. I have not tested the code yet because I plan to work the ideas into my project but it seems to me that with a minor modification to enable automatic abort from state2, this will work...

     

    1.) I am not clear on this line: sm_timer <= (others => '0'); I think we are saying that we assign (others => '0') to sm_timer and that all bits will be 0 because we set nothing else i.e. we did not say something like ('1', '1', others => '0') which would yield '11000'?

     

    2.) Are you using the button_count to check that buttons have been in the same state for some time to act as a debouncer?

     

    4.) Explain why we don't need to reset the timer to zero: Okay, here is my stab... the state machine will process state1 and state2 every 1ms (because although sensitised to the main clock, we use an if statement to process the state machine every 1ms). Because we will only move state when sm_timer reaches "111111", then the next time into the state machine this unsigned sm_timer has wrapped to 0 and so when we finally arrive at state2, sm_timer is 0. the process being clocked means that all these assignments happen at the same time and so we know that the sm_timer will wrap in state1 and we will also assign state2 when in state1 - therefore on the next clock cycle we will be in state2 with sm_timer at 0.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to oldmanraskers

    Hi,

     

    1) The (others => '0') is a good way of setting  a register to zeros and avoids all that tedious counting of how many zeros you've typed, 8 isn't so bad but 96 can get very tiring image

     

    2) Yep, button_count is for debounce

     

    3) I think you've got it - it often causes brain fade - the thing is that although we've passed the line that adds 1 to the sm_timer it doesn't actually happen until after everything else that clock cycle.

     

    The state machine itself is just a demo of how it can be done - you can easily add more states or make them do something useful.

     

    Have fun.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • oldmanraskers
    0 oldmanraskers over 11 years ago in reply to michaelkellett

    image  the code provided by Michael worked for me after I changed the logic states for the switches (the bits needed negating for my board). I will next move onto making the state machine stop at the end of its cycle. I was hoping to post a small video to demonstrate the behaviour but it seems there is something wrong with the video upload image Or is it just me?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to michaelkellett

    Did I miss something? Where is the logic for the state machine? Does it use a clock?

    Clem

    Edited: Ok see it now as attached.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 11 years ago in reply to michaelkellett

    Did I miss something? Where is the logic for the state machine? Does it use a clock?

    Clem

    Edited: Ok see it now as attached.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • johnbeetem
    0 johnbeetem over 11 years ago in reply to clem57

    Clem Martins wrote:

     

    Did I miss something? Where is the logic for the state machine? Does it use a clock?

    Clem

    Edited: Ok see it now as attached.

    I couldn't see the attachment when viewing the discussion in the "Inbox and Activity" page.  I had to open the discussion in a new tab (or window) to see the attachment.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to johnbeetem

    image

    Here's the simulation I did and the testbench that drove it. Simulation in Aldec ActiveHDL, The 1mS time was reduced to 100uS to reduce the simulation cycles.

    There is an attachment as well as the embedded picture !

     

    MK